Hello,
I need to interface a PAL/NTSC Camera with my custom board using iMX8MQ, I try to use ISL79987 with no success.
I'd like to know If there is a Solution with driver compatible with iMX8MQ, ie, just one channel, a format compatible with gst-launch-1.0, and no need of 2D GPU.
Thank you.
Hello Leandro Schmitz,
i.MX8MQ supports 2 MIPI CSI-2 ports, which are camera input interface. so you need to use CVBS to MIPI CSI-2 Bridge for your application, like ADV7280-M. BUT each MIPI CSI-2 of i.MX8MQ can only support 1 channel camera, like this:
(1) MIPI CSI1: 1 camera with PAL/NTSC--->ADV7280-M--->MIPI CSI1
(2) MIPI CSI2: 1 camera with PAL/NTSC--->ADV7280-M--->MIPI CSI2
Hope the information is helpful to you!
Have a nice day!
B.R,
Weidong