Is the pin/pad CSI0_DATA_EN (iMX 6 Quad Core) only option to output ARM clock?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is the pin/pad CSI0_DATA_EN (iMX 6 Quad Core) only option to output ARM clock?

536 次查看
manojprabahar
Contributor I

Is the pin/pad CSI0_DATA_EN only option to output ARM clock off from processor, to ensure that the core is operating at configured speed? Even if so, whether the GPIO is capable to do so? Because when we tried to output the clock via GPIO earlier, it didnt go beyond 400MHz!

标签 (2)
标记 (2)
0 项奖励
1 回复

457 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Manoj

please consider signals CCM_CLKO1, 2 with register CCM_CCOSR (output arm_clk_root)

described in sect.18.6.21 CCM Clock Output Source Register (CCM_CCOSR)

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励