Internal LDO output spec in i.MX6UL/ULL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Internal LDO output spec in i.MX6UL/ULL

616 次查看
ko-hey
Senior Contributor II

Hi all

 

I have a question about accuracy of internal LDOs output in i.MX6UL/ULL.

Could you tell me the spec of internal LDOs output min, typ and max ?

 

Ko-hey

 

标签 (2)
标记 (2)
0 项奖励
3 回复数

464 次查看
art
NXP Employee
NXP Employee

The accuracy of the i.MX6UL/ULL internal LDOs is within one regulation step, i.e. voltage target regulation point +/- 25mV, if not overloaded.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

464 次查看
ko-hey
Senior Contributor II

Hi art

Do you have Max and min spec for LDO_SNVS ?

Ko-hey

0 项奖励

464 次查看
ko-hey
Senior Contributor II

Hi Artur Petukhov

Could you follow the question ?

Ko-hey

0 项奖励