Hello everybody,
I was asked to make a project which requires the fastest access possible to a RAM (write and read).
I am still in a study phase and at the moment it seems to me that the SEMC interface on a i.mx rt 1062 allows to do this.
Has anyone already had experience of this and if so, what type or model of RAM have you used and with what performance?
Thanks
Hello,
Use the following app note:
“i.MX RT Series Performance Optimization”
https://www.nxp.com/docs/en/application-note/AN12437.pdf
Have a great day,
Yuri.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.