Dear Sir,
Our customer used i.MX6UL+ PF3000 and add coin cell to design product.
We knew if system off (PMIC Vin off), coin cell provide power to VSNVS of i.MX6UL then work RTC function only.
If PMIC Vin provide power and system work, we will setting COINCTL register (COINCHEN bit) to enable charger coin cell.
We are not sure how to control disable or know coin cell is full to stop charger.
Could you help provide control method, software or circuit to reference?
Thanks a lot,
Hi Andy
coin cell charger voltage is programmable as described in
sect.6.3.11.4 Coin cell charger control datasheet. It works as
current-limited voltage source, resulting in the CC/CV taper characteristic
typically used for rechargeable Lithium-Ion batteries. So no need
to stop charger current as it stops automatically as cell voltage reaches
programmable level.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------