Initramfs recipe-YOCTO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Initramfs recipe-YOCTO

3,821 Views
michaelwesley
Contributor I

Hi,

I generated initramfs(core-image-minimal-initramfs-imx6ulevk-xxxxx.rootfs.cpio.gz) using core image recipe such as core-image-minimal-initramfs.bb .

From the recipe, package depends on initramfs-live-boot, initramfs-live-install, initramfs-live-install-efi, so what is the major difference between boot, install & efi script. Did i need all the three?

Also, while booting initramfs, i'm getting the following error,

Freeing unused kernel memory: 412K (80a45000 - 80aac000)
mount: mounting /run/media///rootfs.img on /rootfs/ failed: No such file or directory
/init: line 196: can't create : nonexistent directory
/init: line 196: can't create : nonexistent directory
sh: can't access tty; job control turned off
/ #
/ #

Kindly share your thoughts.

Labels (2)
Tags (2)
0 Kudos
1 Reply

1,708 Views
igorpadykov
NXP Employee
NXP Employee

Hi Michael

one can look at

Yocto initramfs 

regarding dependencies may be recommended to post

on yocto project mail list as this is generic yocto question

Mailing Lists | Yocto Project 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos