Hi all,
We are using imx6solo custom board. In this we have MMPF100 - pmic IC. I configure this pmic in uboot and kernel also. i got the PMIC detecetion log in uboot and kernel also.
In u-boot log:
U-Boot 2014.04-08637-gaffa032-dirty (May 20 2016 - 16:28:07)
CPU: Freescale i.MX6SOLO rev1.1 at 792 MHz
CPU: Temperature 31 C, calibration data: 0x5444cf5f
Reset cause: POR
Board: MX6-SabreSD
I2C: readyf
DRAM: 1 GiB
MMC: ***case 0***
FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
***get_cd==case 2***
*** Warning - bad CRC, using default environment
No panel detected: default to HDMI
Display: HDMI (1920x1080)
In: serial
Out: serial
Err: serial
** Found PFUZE100 deviceid=10,revid=21
unsupported boot devices
check_and_clean: reg 0, flag_set 0
Fastboot: Normal
flash target is MMC:1
***get_cd==case 2***
Net: $$$$$$$$$$$$$$$$$$$$$$$$$$$$$
Phy not found
PHY reset timed out
FEC [PRIME]
Warning: failed to set MAC address
Kernel log:
pfuze100-regulator 0-0008: Full lay: 2, Metal lay: 1
pfuze100-regulator 0-0008: FAB: 0, FIN: 0
pfuze100-regulator 0-0008: pfuze100 found.
SW1AB: 300 <--> 1875 mV at 1375 mV
SW1C: 300 <--> 1875 mV at 1375 mV
SW2: 800 <--> 3300 mV at 3300 mV
SW3A: 400 <--> 1975 mV at 1500 mV
SW3B: 400 <--> 1975 mV at 1500 mV
SW4: 800 <--> 3300 mV at 3150 mV
SWBST: 5000 <--> 5150 mV at 5000 mV
VSNVS: 1000 <--> 3000 mV at 3000 mV
VREFDDR: 750 mV
VGEN1: 800 <--> 1550 mV at 1500 mV
VGEN2: 800 <--> 1550 mV at 1500 mV
VGEN3: 1800 <--> 3300 mV at 2800 mV
VGEN4: 1800 <--> 3300 mV at 1800 mV
VGEN5: 1800 <--> 3300 mV at 3000 mV
VGEN6: 1800 <--> 3300 mV at 3300 mV
Serial: IMX driver
From boot log i think PMIC configuration is proper. But we check in hardware the voltage is not reduced and also processor is heating.
How to fix it??
Regards,
Aravinth
已解决! 转到解答。
if correct board configuration is selected, refer to attached Linux Guide
sect.5 Enabling Solo Emulation, no need for any code changes.
Using mfg tools, configuration mfgtool2-android-mx6dl-sabresd-sd.vbs
should be used. Seems you can debug it, adding printfs to cpufreq driver.
~igor
Hi igorpadykov,
Thanks for your response.
Now i am able to get "SW1AB: 300 <--> 1875 mV at 1175 mV" in my custom board also.
In EVK after kernel up SW1AB always in 1175 mV only. Android goes to sleep mode in evk SW1AB reduced to 0.9 V.
but in our custom board after kernel up after few seconds later SW1AB goes to 1275 mV. And android goes to sleep mode in custom board SW1AB back to 1175 mV.
How to hold SW1AB in 1175 mV in active state and SW1AB in 0.9 V in sleep mode.??
Regards,
Aravinth
Hi aravinthkumar
could you try linux below (also with U-Boot 2014.04 version), will it work
Board Support Packages (38)
L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)
what android used in the case, it is from official nxp product page ?
SABRE Board Reference Design|NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
EVK board PMIC kernel log:
pfuze100-regulator 1-0008: Full lay: 1, Metal lay: 1
pfuze100-regulator 1-0008: FAB: 0, FIN: 0
pfuze100-regulator 1-0008: pfuze100 found.
SW1AB: 300 <--> 1875 mV at 1175 mV
SW1C: 300 <--> 1875 mV at 1175 mV
Custom board PMIC Kernel log:
pfuze100-regulator 0-0008: Full lay: 2, Metal lay: 1
pfuze100-regulator 0-0008: FAB: 0, FIN: 0
pfuze100-regulator 0-0008: pfuze100 found.
SW1AB: 300 <--> 1875 mV at 1375 mV
SW1C: 300 <--> 1875 mV at 1375 mV
How to reduce this SW1AB: 300 <--> 1875 mV at 1375 mV into SW1AB: 300 <--> 1875 mV at 1175 mV ??
Where i need to configure this 1375 -> 1175 voltagein kernel .??
Regards,
Aravinth
what bsp are you using ?
>Where i need to configure this 1375 -> 1175 voltagein kernel .?
these voltages are set by CPU Frequency Scaling (CPUFREQ) Driver,
it is just necessary to use correct image for board. Description can be found
in Linux/Android documentation included in bsp.
~igor
Hi igorpadykov,
I'm using freescale android 4.4.3 bsp.
In EVK board log we got "SW1AB: 300 <--> 1875 mV at 1175 mV", but in our custom board we got "SW1AB: 300 <--> 1875 mV at 1375 mV" .And also Our processor is heating. So i need to make 1375 mV into 1175 mV in our custom board.
How to do this..?
Regards,
Aravinth