Hello,
we have designed a customized board with imx8mmevk processor and we are testing for thermal shock test from -40 degree C to +85 degree C (Dwell Time is 2 hrs and ramp time is 1 to 3 minute). Under this the processor is shutting it self between +75 degree C to +85 degree C. Please find the attached log
how to ensure that the processor doesnt shutdown when this is reaching at 85 degree C
Regards
santhosh
You can configure shutdown temperature in Linux.
Please refer to chapter 2.9 "Thermal" of i.MX Linux Reference Manual.
Yes I changed as per the settings but the processor CPU temperature is reaching 100 degree C when the environmental chamber temperature is 75 Deg C
cat /sys/devices/virtual/thermal/thermal_zone0/temp
Used the above command to get the CPU temperature
Regards
Santhosh
Please look at the patch in this thread:
https://community.nxp.com/t5/i-MX-Processors/i-mx8mm-cpureq-cooling-issue/m-p/1176540
Maybe it helps.