Imx8 Mini with MX8 DSI OLED

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx8 Mini with MX8 DSI OLED

22 Views
Alirezah95
Contributor II

Hi

I have a *MX8 DSI OLED1* display which I want to use with IMX8 Mini. I've started the board with the default os on MMC and loaded the rm67191 dtb from uboot, lcd is showing the image but there is a strange issue with it displaying two colors on the screen as can be seen in the attached image. This is also the case for a custom OS built using Yocto. How can I solve this issue?

Regards.

photo_2024-07-17_20-23-27.jpg

Tags (1)
0 Kudos
Reply
0 Replies