Hello my name is françois,
I work with im7dsabresd, I want use the graphical back frame buffer with qt5. I build a core-image-minimal but I have an error:
| /opt/fsl-jethro-bsp/build/tmp/sysroots/x86_64-linux/usr/libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/5.2.0/ld: cannot find -lGL
| collect2: error: ld returned 1 exit status
| make: *** [opengldesktop] Error 1
| OpenGL disabled.
| The OpenGL functionality test failed!
| You might need to modify the include and library search paths by editing
| QMAKE_INCDIR_OPENGL, QMAKE_LIBDIR_OPENGL and QMAKE_LIBS_OPENGL in
| /opt/fsl-jethro-bsp/build/tmp/work/cortexa7hf-vfp-neon-poky-linux-gnueabi/qtbase/5.5.1+gitAUTOINC+5afc431323-r0/git/mkspecs/linux-oe-g++.
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_configure (log file is located at /opt/fsl-jethro-bsp/build/tmp/work/cortexa7hf-vfp-neon-poky-linux-gnueabi/qtbase/5.5.1+gitAUTOINC+5afc431323-r0/temp/log.do_configure.20189)
ERROR: Task 416 (/opt/fsl-jethro-bsp/sources/meta-qt5/recipes-qt/qt5/qtbase_git.bb, do_configure) failed with exit code '1'
I don't understand this error can you help me please.
I attache my bblayer et local file and the log file.
Thanks for All Help.
Best regards
François.
Recommandation (0) • Commenter • Partager
Original Attachment has been moved to: log.do_configure.20189.zip
Original Attachment has been moved to: local.conf.zip
Original Attachment has been moved to: bblayers.conf.zip
Hi François
seems qt5 images are not supported for i.MX 6UltraLite and i.MX 7Dual
(note they have not vpu/gpu) as mentioned in attached Yocto Guide
Table 1. Freescale Yocto project images
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov
Ok to fsl_image_qt5. But I use a core-image-minimal and in my local.conf, I don't use qt qml or qt quick.
If there is not solution this means that nobody can use QT5 with imx7 dual, it is a very bad news.
Best regards
françois.
it may be used but without gpu accelerator, just with software,
please look at:
Qt5 on embedded systems without GPU/OpenGL | Qt Forum
~igor