Dear my friends
I would like to modify the uboot emmc driver so that it supports dma boot ,because i think it takes a lot of time to load the kernel and ramdisk image
In fact, my real goal is to save boot time, I have cut off a lot of useless drivers, but still need about 480ms time. So I hope uboot starting from emmc using DMA. At the same time I need to know if it can save some time
Ihope someone can give me some help or some of the views, I can do to achieve the goal .
Thank you
解決済! 解決策の投稿を見る。
Hi zhuchao
actually i.MX6DQP uSDHC module has own dma engine, please
refer to Figure 68-1. System Connection of the uSDHC i.MX6DQP Reference Manual
http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Here are some general hints for booting under one second:
Booting i.MX6 under one second - i.MXDev Blog
Also, U-Boot 2017.03 has an improvement for the copy (cp command) implementation based on assembly library.
If you use cp command in U-Boot you may consider moving to the latest U-Boot version.
Hi zhuchao
actually i.MX6DQP uSDHC module has own dma engine, please
refer to Figure 68-1. System Connection of the uSDHC i.MX6DQP Reference Manual
http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------