Imx6 custom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
847件の閲覧回数
bastien
Contributor I

Hello comminity,

I am working on imx6 custom board and i want to add ethernet interface.

The evaluations boards from nxp are based on RGMII with AR8031 chip or lan8720.

I need to know :

Does the linux recognizes automatically the phy ethernet even if I choose an other phy components as the ksz8794 or others ?

If driver is needed, how to build and implement it on my custol software?

Is it possible to get some documentations about this ?

Thank you

Best regards

0 件の賞賛
返信
1 解決策
833件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi bastien

 

some specific for each phy ethernet can be required, as for example related to ar8031 codes can be

found in .. arch/arm/mach-imx/mach-imx6q.c, drivers/net/ethernet/freescale/fec_fixup.c
for lan8720 in ..drivers/net/phy/smsc.c :

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/net/phy?h=imx_4.19.35_1.1.0&id=2a8...

Porting documentation can be found in

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
834件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi bastien

 

some specific for each phy ethernet can be required, as for example related to ar8031 codes can be

found in .. arch/arm/mach-imx/mach-imx6q.c, drivers/net/ethernet/freescale/fec_fixup.c
for lan8720 in ..drivers/net/phy/smsc.c :

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/net/phy?h=imx_4.19.35_1.1.0&id=2a8...

Porting documentation can be found in

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 件の賞賛
返信