Hi ,
I am working IMX6ULL EVK , I have develop my application,
how I can auto start my application at startup before login ?
I see forums that modify /etc/inittab file, but in my file system this file there isn't.
I compile my SD image with 'core-image-base' option.
Do I must append other modules ?
At the moment I put the start of my application inside /etc/profile, but at startup I must put login and than the application start.
Can someone help me ?
Sergio
Hi Victor,
thank you for answer,
the file /etc/rc.local in my file system not exist. I send you my /etc foulder ls -l :
root@imx6ull14x14evk:/etc# ls -l
-rw-r--r-- 1 root root 5281 Jul 25 2019 asound.conf
drwxr-xr-x 3 root root 1024 Oct 1 2019 avahi
drwxr-xr-x 2 root root 1024 Oct 1 2019 bluetooth
-rw-r--r-- 1 root root 2314 Jul 25 2019 busybox.links.nosuid
-rw-r--r-- 1 root root 91 Jul 25 2019 busybox.links.suid
drwxr-xr-x 3 root root 1024 Oct 1 2019 ca-certificates
-rw-r--r-- 1 root root 6115 Jul 25 12:44 ca-certificates.conf
drwxr-xr-x 3 root root 1024 Oct 1 2019 dbus-1
drwxr-xr-x 3 root root 1024 Oct 1 2019 default
drwxr-xr-x 2 root root 1024 Jul 25 2019 depmod.d
drwxr-xr-x 3 root root 1024 Oct 1 2019 dnf
-rw-r--r-- 1 root root 38 Jul 25 12:30 filesystems
drwxr-xr-x 2 root root 1024 Oct 1 2019 firmware
-rw-r--r-- 1 root root 637 Jul 25 12:30 fstab
-rw-r--r-- 1 root root 747 Jul 25 12:32 group
-rw-r--r-- 1 root root 737 Jul 25 12:32 group-
-r-------- 1 root root 630 Jul 25 12:32 gshadow
-r-------- 1 root root 620 Jul 25 12:32 gshadow-
-rw-r--r-- 1 root root 26 Jul 25 12:30 host.conf
-rw-r--r-- 1 root root 16 Jul 25 12:30 hostname
-rw-r--r-- 1 root root 237 Jul 25 2019 hosts
-rw-r--r-- 1 root root 1633 Jul 25 2019 inputrc
-rw-r--r-- 1 root root 41 Jul 25 12:30 issue
-rw-r--r-- 1 root root 38 Jul 25 12:30 issue.net
-rw-r--r-- 1 root root 6577 Jul 25 12:32 ld.so.cache
-rw-r--r-- 1 root root 0 Oct 1 2019 ld.so.conf
drwxr-xr-x 2 root root 1024 Oct 1 2019 libnl
-rw-r--r-- 1 root root 11595 Jul 26 2019 lighttpd.conf
drwxr-xr-x 2 root root 1024 Jul 26 2019 lighttpd.d
-rw-r--r-- 1 root root 827 Jul 25 2019 limits
-rw-r--r-- 1 root root 2006 Jul 25 2019 login.access
-rw-r--r-- 1 root root 10929 Jul 25 2019 login.defs
-rw-r--r-- 1 root root 33 Jul 25 12:32 machine-id
drwxr-xr-x 2 root root 1024 Jul 25 2019 modprobe.d
drwxr-xr-x 2 root root 1024 Jul 25 2019 modules-load.d
-rw-r--r-- 1 root root 0 Jul 25 12:30 motd
lrwxrwxrwx 1 root root 12 Jul 25 12:30 mtab -> /proc/mounts
-rw-r--r-- 1 root root 767 Jul 25 2019 netconfig
drwxr-xr-x 5 root root 1024 Oct 1 2019 network
-rw-r--r-- 1 root root 514 Oct 1 2019 nsswitch.conf
drwxr-xr-x 2 root root 1024 Oct 1 2019 ofono
lrwxrwxrwx 1 root root 21 Jul 25 12:40 os-release -> ../usr/lib/os-release
drwxr-xr-x 2 root root 1024 Oct 1 2019 pam.d
-rw-r--r-- 1 root root 1096 Oct 1 2019 passwd
-rw-r--r-- 1 root root 913 Jul 25 12:33 profile
-rw-r--r-- 1 root root 2932 Jul 25 2019 protocols
drwxr-xr-x 2 root root 1024 Jul 25 12:32 pulse
lrwxrwxrwx 1 root root 34 Jul 25 2019 resolv-conf.systemd -> ../run/systemd/resolve/resolv.
conf
lrwxrwxrwx 1 root root 24 Oct 1 2019 resolv.conf -> /etc/resolv-conf.systemd
-rw-r--r-- 1 root root 895 Jul 25 2019 rpc
-rwxr-xr-x 1 root root 58 Jul 25 2019 rpcbind.conf
drwxr-xr-x 2 root root 1024 Oct 1 2019 rpm
-rw-r--r-- 1 root root 340 Oct 1 2019 rpmrc
-r-------- 1 root root 1848 Jul 25 12:40 securetty
-rw-r--r-- 1 root root 19199 Jul 25 2019 services
-r-------- 1 root root 702 Oct 1 2019 shadow
-rw-r--r-- 1 root root 42 Jul 25 12:30 shells
drwxr-xr-x 2 root root 1024 Oct 1 2019 skel
drwxr-xr-x 4 root root 1024 Jul 25 12:44 ssl
drwxr-xr-x 2 root root 1024 Jul 25 2019 sysctl.d
-rw-r--r-- 1 root root 69 Jul 25 2019 syslog.conf
drwxr-xr-x 5 root root 1024 Oct 1 2019 systemd
drwxr-xr-x 9 root root 1024 Oct 1 2019 terminfo
-rw-r--r-- 1 root root 15 Oct 1 2019 timestamp
drwxr-xr-x 2 root root 1024 Oct 1 2019 tmpfiles.d
drwxr-xr-x 4 root root 1024 Jul 25 12:32 udev
drwxr-xr-x 2 root root 1024 Oct 1 2019 udhcpc.d
-rw-r--r-- 1 root root 15 Oct 1 2019 version
-rw------- 1 root root 113 Jul 25 2019 wpa_supplicant.conf
drwxr-xr-x 3 root root 1024 Oct 1 2019 xdg
root@imx6ull14x14evk:/etc#
Perhaps do some other module need included ?
I have do bitbake with 'core-image-base' option.
Have you an other suggestion ?
Sergio.
Alternativelly you can place your script into /etc/init.d
root@imx8qmmek:/etc/init.d# cat test.sh
#!/bin/sh
echo test > /file.txt
root@imx8qmmek:/etc/init.d# ls -l test.sh
-rwxr-xr-x 1 root root 22 May 25 18:50 test.sh
root@imx8qmmek:/etc/init.d#
and add it into exact runlevel:
root@imx8qmmek:/etc/init.d# runlevel
N 3
root@imx8qmmek:/etc/init.d# cd /etc/rc3.d/
root@imx8qmmek:/etc/rc3.d# ln -s ../init.d/test.sh S50test.sh
root@imx8qmmek:/etc/rc3.d#
Hi Victor,
your example work well, the file .txt is create at start up automatically.
But when I add or substitute with "echo ./test_software" the program not start. (if I lunch ./test_software after login the program start well).
Have you other suggestion ?
Sergio.