Imx53 Android 4.0.4 (linaro source) wifi GUI issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Imx53 Android 4.0.4 (linaro source) wifi GUI issue

1,134 次查看
swaraj
Contributor II
Hi, I am building android 4.0.4 for imx53 board. I'm stuck with wifi porting issue. I'm able to scan and connect using command prompt, but i'm unable to use GUI for wlan0 and not able to start supplicant properly with GUI. The following is the error message: D/NetworkManagementService( 1144): Registering observer I/WifiService( 1144): WifiService starting up with Wi-Fi enabled I/WifiHW ( 1144): ************* wifi.c insmod is called********** I/ethernet( 1144): User ask for device name on 0, list:B7F740, total:2 I/ethernet( 1144): User ask for device name on 1, list:B7F740, total:2 I/WifiHW ( 1144): ************* wifi.c insmod is called********** D/NetworkManagementService( 1144): rsp <213 00:23:a7:00:01:58 0.0.0.0 0 [down broadcast multicast]> D/CommandListener( 1066): Setting iface cfg D/CommandListener( 1066): Trying to bring down wlan0 D/CommandListener( 1066): broadcast flag ignored D/CommandListener( 1066): multicast flag ignored D/NetworkManagementService( 1144): flags <[down broadcast multicast]> E/WifiHW ( 1144): ctrl_interface is = /data/misc/wifi E/WifiHW ( 1144): Unable to open connection to supplicant on "wlan0": E/WifiHW ( 1144): Unable to open connection to supplicant on "wlan0": No such file or directory E/WifiHW ( 1144): Unable to open connection to supplicant on "wlan0": E/WifiHW ( 1144): Unable to open connection to supplicant on "wlan0": No such file or directory W/EthernetStateMachine( 1144): Could not stop DHCP I/EthernetSta[ 66.122325] init: no such service 'dhcpcd_sit0:-h android-45fe3c772cef2905 sit0' teMachine( 1144): trigger dhcp for device sit0 I/SystemServer( 1144): Throttle Service E/WifiHW ( 1144): Unable to open connection to supplicant on "wlan0": E/WifiHW ( 1144): Unable to open connection to supplicant on "wlan0": No such file or directory I/SystemServer( 1144): Backup Service D/dalvikvm( 1144): GC_CONCURRENT freed 182K, 4% free 8037K/8327K, paused 3ms+47ms I/SystemServer( 1144): SamplingProfiler Service E/WifiHW ( 1144): Unable to open connection to supplicant on "wlan0": E/WifiHW ( 1144): Unable to open connection to supplicant on "wlan0": No such file or directory I/SystemServer( 1144): NetworkTimeUpdateService I/WindowManager( 1144): SAFE MODE not enabled W/RecognitionManagerService( 1144): no available voice recognition services found E/WifiHW ( 1144): Unable to open connection to supplicant on "wlan0": E/WifiHW ( 1144): Unable to open connection to supplicant on "wlan0": No such file or directory D/dalvikvm( 1144): GC_CONCURRENT freed 252K, 4% free 8311K/8647K, paused 5ms+5ms I/ActivityManager( 1144): Start proc org.linaro.wallpaper for service org.linaro.wallpaper/.LogoWallpaper: pid=1236 uid=10019 gids={} W/InputManagerService( 1144): Ignoring setImeWindowStatus of uid 1000 token: null E/WifiHW ( 1144): Unable to open connection to supplicant on "wlan0": E/WifiHW ( 1144): Unable to open connection to supplicant on "wlan0": No such file or directory E/WifiStateMachine( 1144): Failed to setup control channel, restart supplicant I/ActivityManager( 1144): Start proc com.android.inputmethod.latin for service com.android.inputmethod.latin/.LatinIME: pid=1248 uid=10028 gids={} D/SystemUIService( 1221): loading: class com.android.systemui.statusbar.tablet.TabletStatusBar D/SystemUIService( 1221): running: com.android.systemui.statusbar.tablet.TabletStatusBar@4112ff98 sms: com.android.providers.telephony.MmsSmsProvider I/Process ( 1144): Sending signal. PID: 1298 SIG: 3 I/dalvikvm( 1298): threadid=3: reacting to signal 3 I/wpa_supplicant( 1315): CTRL-EVENT-STATE-CHANGE id=-1 state=2 BSSID=00:00:00:00:00:00 [ 76.900519] SIOCSIWPRIV request wlan0, info->cmd:8b0c, info->flags:0 [ 76.900532] dwrq->length:20E/WifiHW ( 1144): Unable to open connection to supplicant on "wlan0": E/WifiHW ( 1144): Unable to open connection to supplicant on "wlan0": No such file or directory In wifi.c file i included few changes: //static const char IFACE_DIR[] = "/data/system/wpa_supplicant"; //#ifdef WIFI_DRIVER_MODULE_PATH //static const char DRIVER_MODULE_NAME[] = WIFI_DRIVER_MODULE_NAME; static const char DRIVER_MODULE_TAG[] = WIFI_DRIVER_MODULE_NAME " "; //static const char DRIVER_MODULE_PATH[] = WIFI_DRIVER_MODULE_PATH; static const char DRIVER_MODULE_ARG[] = WIFI_DRIVER_MODULE_ARG; //#endif static const char FIRMWARE_LOADER[] = WIFI_FIRMWARE_LOADER; static const char DRIVER_PROP_NAME[] = "wlan.driver.status"; static const char SUPPLICANT_NAME[] = "wpa_supplicant"; static const char SUPP_PROP_NAME[] = "init.svc.wpa_supplicant"; static const char SUPP_CONFIG_TEMPLATE[]= "/system/etc/wifi/wpa_supplicant.conf"; static const char SUPP_CONFIG_FILE[] = "/data/misc/wifi/wpa_supplicant.conf"; static const char P2P_CONFIG_FILE[] = "/data/misc/wifi/p2p_supplicant.conf"; static const char CONTROL_IFACE_PATH[] = "/data/misc/wifi"; static const char MODULE_FILE[] = "/proc/modules"; static const char SUPP_ENTROPY_FILE[] = WIFI_ENTROPY_FILE; static unsigned char dummy_key[21] = { 0x02, 0x11, 0xbe, 0x33, 0x43, 0x35, 0x68, 0x47, 0x84, 0x99, 0xa9, 0x2b, 0x1c, 0xd3, 0xee, 0xff, 0xf1, 0xe2, 0xf3, 0xf4, 0xf5 }; In init.rc i made following modifications: mkdir /data/misc/systemkeys 0700 system system mkdir /data/misc/vpn/profiles 0770 system system # give system access to wpa_supplicant.conf for backup and restore mkdir /data/misc/wifi 0770 wifi wifi chmod 0770 /data/misc/wifi chmod 0777 /data/misc/wifi/wpa_supplicant chmod 0777 /system/release mkdir /data/misc/wifi/sockets 0777 wifi wifi chmod 0667 /data/misc/wifi/wpa_supplicant.conf chmod 0777 /system/release/wifi_settings.cfg mkdir /data/local 0751 root root mkdir /data/local/tmp 0771 shell shell mkdir /data/data 0771 system system mkdir /data/app-private 0771 system system mkdir /data/app 0771 system system mkdir /data/property 0700 root root chmod 0777 /system/release setprop wifi.interface wlan0 #setprop wlan.driver.status "ok" #Define service for wifi #service wpa_supplicant /system/bin/wpa_supplicant -Drsi -iwlan0 -c/system/release/wifi_settings.cfg #service wpa_supplicant /system/bin/wpa_supplicant -Drsi -iwlan0 -c/data/misc/wifi/wpa_supplicant.conf service wpa_supplicant /system/bin/wpa_supplicant -Dwext -iwlan0 -c/data/misc/wifi/wpa_supplicant.conf group system wifi inet disabled oneshot service ifcfg_eth /system/bin/ifconfig wlan0 up disabled oneshot #service dhcpcd_wlan0 /system/bin/dhcpcd -BKL wlan0 -f /system/etc/android.conf service dhcpcd_wlan0 /system/bin/dhcpcd -BKL wlan0 group system dhcp disabled oneshot
标签 (1)
标记 (2)
0 项奖励
回复
0 回复数