Imx51 can not jump to image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx51 can not jump to image

1,118 Views
huzizhen
Contributor I

all:

     imx51,wince6.0 R3,WCE600_11.04.02_ER.

     I build nk.nb0,it can work good.but i add a *.exe file to image,it can not jump to image as follow logs.

INFO: Using device name: 'MX5165535'

INFO: Reading NK image to SDHC (please wait)...

INFO:  dwActualLength = [0x2339034]

INFO: Copying NK image to RAM address 0xa0200000

 

 

INFO: Read is 1% complete

INFO: Read is 2% complete

INFO: Read is 3% complete

INFO: Read is 4% complete

INFO: Read is 5% complete

INFO: Read is 6% complete

INFO: Read is 7% complete

INFO: Read is 8% complete

INFO: Read is 9% complete

INFO: Read is 10% complete

INFO: Read is 11% complete

INFO: Read is 12% complete

INFO: Read is 13% complete

INFO: Read is 14% complete

INFO: Read is 15% complete

INFO: Read is 16% complete

INFO: Read is 17% complete

INFO: Read is 18% complete

INFO: Read is 19% complete

INFO: Read is 20% complete

INFO: Read is 21% complete

INFO: Read is 22% complete

INFO: Read is 23% complete

INFO: Read is 24% complete

INFO: Read is 25% complete

INFO: Read is 26% complete

INFO: Read is 27% complete

INFO: Read is 28% complete

INFO: Read is 29% complete

INFO: Read is 30% complete

INFO: Read is 31% complete

INFO: Read is 32% complete

INFO: Read is 33% complete

INFO: Read is 34% complete

INFO: Read is 35% complete

INFO: Read is 36% complete

INFO: Read is 37% complete

INFO: Read is 38% complete

INFO: Read is 39% complete

INFO: Read is 40% complete

INFO: Read is 41% complete

INFO: Read is 42% complete

INFO: Read is 43% complete

INFO: Read is 44% complete

INFO: Read is 45% complete

INFO: Read is 46% complete

INFO: Read is 47% complete

INFO: Read is 48% complete

INFO: Read is 49% complete

INFO: Read is 50% complete

INFO: Read is 51% complete

INFO: Read is 52% complete

INFO: Read is 53% complete

INFO: Read is 54% complete

INFO: Read is 55% complete

INFO: Read is 56% complete

INFO: Read is 57% complete

INFO: Read is 58% complete

INFO: Read is 59% complete

INFO: Read is 60% complete

INFO: Read is 61% complete

INFO: Read is 62% complete

INFO: Read is 63% complete

INFO: Read is 64% complete

INFO: Read is 65% complete

INFO: Read is 66% complete

INFO: Read is 67% complete

INFO: Read is 68% complete

INFO: Read is 69% complete

INFO: Read is 70% complete

INFO: Read is 71% complete

INFO: Read is 72% complete

INFO: Read is 73% complete

INFO: Read is 74% complete

INFO: Read is 75% complete

INFO: Read is 76% complete

INFO: Read is 77% complete

INFO: Read is 78% complete

INFO: Read is 79% complete

INFO: Read is 80% complete

INFO: Read is 81% complete

INFO: Read is 82% complete

INFO: Read is 83% complete

INFO: Read is 84% complete

INFO: Read is 85% complete

INFO: Read is 86% complete

INFO: Read is 87% complete

INFO: Read is 88% complete

INFO: Read is 89% complete

INFO: Read is 90% complete

INFO: Read is 91% complete

INFO: Read is 92% complete

INFO: Read is 93% complete

INFO: Read is 94% complete

INFO: Read is 95% complete

INFO: Read is 96% complete

INFO: Read is 97% complete

INFO: Read is 98% complete

INFO: Read is 99% complete

INFO: Read is 100% complete

INFO: Copy of NK completed successfully

Download successful!  Jumping to image at 0x0 (physical 0x90200000)...

 

it stoped.

 

the attach file is my config.bib,and i add a line

GrestCfg.exe        $(_FLATRELEASEDIR)\GrestCfg.exe         NK    U

 

the grestcfg.exe is 149KB.

are someone give me some advances,thanks.

Original Attachment has been moved to: config.bib.zip

Labels (2)
0 Kudos
Reply
5 Replies

897 Views
jimmychan
NXP TechSupport
NXP TechSupport

I cannot find the GrestCfg.exe in your file. and what is the GrestCfg.exe used for?

0 Kudos
Reply

897 Views
huzizhen
Contributor I

Sorry,it is platform.bib.

Because my hive-base registry can not work,so i added a app to save touch data.

0 Kudos
Reply

897 Views
jimmychan
NXP TechSupport
NXP TechSupport

If the booting stop because of this grestcfg.exe, then obviously this is not a problem of i.mx51 or wince drivers. the problem is in this grestcfg.exe. What I can suggest you is to debug this grestcfg.exe. :smileyhappy:

0 Kudos
Reply

897 Views
huzizhen
Contributor I

Hi jjimmychan:

   I can not find why the system stop.

   I do not modifty anything but rebuild and clean sysgen,the nk.nb0 can work good.

   But when i modifty locale to chianese(simplified),after build,it stoped as the same msg.

0 Kudos
Reply

897 Views
huzizhen
Contributor I

the app can work good with wince6.0

0 Kudos
Reply