Hi, I have a custom board based on imx28evk that I'm tring to boot using ubifs for the filesystem
but It doesn't work, I'm using linux 2.6.35.3 with yocto, I have tried this steps
flash_erase /dev/mtd2 0 0
ubiformat /dev/mtd2 -f /core-image-my.ubi
ubiattach /dev/ubi_ctrl -m 2
sync
mount -t ubifs /dev/ubi0_0 /mnt/ubifs
ls -l /mnt/ubifs
Until this point all the things works but when a try to boot the board I get this
Boot area protection is enabled.
Creating 5 MTD partitions on "gpmi-nfc-main":
0x000000000000-0x000001000000 : "nand.bootloader"
0x000001000000-0x000002000000 : "nand.kernel.0"
0x000002000000-0x000010600000 : "nand.rootfs.0"
0x000010600000-0x000011600000 : "nand.kernel.1"
0x000011600000-0x00001fc00000 : "nand.rootfs.1"
UBI: attaching mtd2 to ubi0
UBI: physical eraseblock size: 131072 bytes (128 KiB)
UBI: logical eraseblock size: 126976 bytes
UBI: smallest flash I/O unit: 2048
UBI: VID header offset: 2048 (aligned 2048)
UBI: data offset: 4096
UBI: attached mtd2 to ubi0
UBI: MTD device name: "nand.rootfs.0"
UBI: MTD device size: 230 MiB
UBI: number of good PEBs: 1840
UBI: number of bad PEBs: 0
UBI: max. allowed volumes: 128
UBI: wear-leveling threshold: 4096
UBI: number of internal volumes: 1
UBI: number of user volumes: 1
UBI: available PEBs: 0
UBI: total number of reserved PEBs: 1840
UBI: number of PEBs reserved for bad PEB handling: 18
UBI: max/mean erase counter: 1/0
UBI: image sequence number: 965744890
UBI: background thread "ubi_bgt0d" started, PID 34
UBI error: ubi_init: cannot attach mtd2
ubiblka: unknown partition table
FEC Ethernet Driver
fec_enet_mii_bus: probed
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci: irq 93, io base 0x80080000
fsl-ehci fsl-ehci: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.0: irq 92, io base 0x80090000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
ARC USBOTG Device Controller driver (1 August 2005)
mice: PS/2 mouse device common for all mice
input: matrix-keypad as /devices/platform/matrix-keypad.0/input/input0
input: MXS touchscreen as /devices/virtual/input/input1
MXS RTC driver v1.0 hardware v2.3.0
mxs-rtc mxs-rtc.0: rtc core: registered mxs-rtc as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
Linux video capture interface: v2.00
mxs-pxp mxs-pxp.0: initialized
WARNING : No battery connected !
Aborting power driver initialization
mxs-battery: probe of mxs-battery.0 failed with error 1
mxs watchdog: initialized, heartbeat 19 sec
mxs-mmc: MXS SSP Controller MMC Interface driver
mxs-mmc mxs-mmc.0: mmc0: MXS SSP MMC DMAIRQ 82 ERRIRQ 96
dcp dcp.0: DCP crypto enabled.!
usbcore: registered new interface driver hiddev
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
sgtl5000_hw_read: read reg error : Reg 0x00
Device with ID register 0 is not a SGTL5000
mxs-spdif mxs-spdif.0: MXS SPDIF Audio Transmitter
No device for codec mxs spdif
No device for DAI mxs spdif
No device for DAI mxs-saif
No device for DAI mxs-spdif
asoc: mxs spdif <-> mxs-spdif mapping ok
ALSA device list:
#0: mxs-evk (mxs spdif)
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
802.1Q VLAN Support v1.8 Ben Greear <greearb@candelatech.com>
All bugs added by David S. Miller <davem@redhat.com>
mxs-rtc mxs-rtc.0: setting system clock to 2014-02-13 03:54:32 UTC (1392263672)
eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=0:00, irq=-1)
IP-Config: Complete:
device=eth0, addr=192.168.40.32, mask=255.255.255.0, gw=255.255.255.255,
host=192.168.40.32, domain=, nis-domain=(none),
bootserver=192.168.40.1, rootserver=192.168.40.1, rootpath=
UBIFS: mounted UBI device 0, volume 0, name "imx28_asga_analit-rootfs"
UBIFS: file system size: 229445632 bytes (224068 KiB, 218 MiB, 1807 LEBs)
UBIFS: journal size: 9023488 bytes (8812 KiB, 8 MiB, 72 LEBs)
UBIFS: media format: w4/r0 (latest is w4/r0)
UBIFS: default compressor: lzo
UBIFS: reserved for root: 0 bytes (0 KiB)
VFS: Mounted root (ubifs filesystem) on device 0:15.
devtmpfs: mounted
Freeing init memory: 160K
INIT: version 2.88 booting
PHY: 0:00 - Link is Up - 100/Full
Starting udev
<30>udevd[135]: starting version 182
Unable to handle kernel paging request at virtual address fffffff0
pgd = c0004000
[fffffff0] *pgd=407b5031, *pte=00000000, *ppte=00000000
Internal error: Oops: 17 [#1] PREEMPT
last sysfs file: /sys/devices/virtual/tty/ptydf/uevent
Modules linked in:
CPU: 0 Not tainted (2.6.35.3+yocto #4)
PC is at ubi_leb_read+0x10/0x124
LR is at ubiblock_readsect+0xbc/0xec
pc : [<c0298f44>] lr : [<c029f998>] psr: 60000013
sp : cf46ff18 ip : cf46ff50 fp : cf46ff4c
r10: 0001f000 r9 : 00000000 r8 : cf21d400
r7 : 00000400 r6 : 00000200 r5 : 00000200 r4 : cff9cea0
r3 : 00000400 r2 : cf21d400 r1 : 00000000 r0 : fffffff0
Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 0005317f Table: 4f5e4000 DAC: 00000017
Process ubiblk2 (pid: 35, stack limit = 0xcf46e270)
Stack: (0xcf46ff18 to 0xcf470000)
ff00: c03f1304 cff9cea0
ff20: c029f8dc cf21d400 cf46ff4c cff9cea0 00000200 00000200 00000400 cf21d400
ff40: cf46ff84 cf46ff50 c029f998 c0298f44 00000200 00000000 00000000 00000000
ff60: c029f8dc cf21d400 c0551700 cfdcf410 cff9cf00 cf46e000 cf46ffc4 cf46ff88
ff80: c02747d0 c029f8ec cff953f0 cff9cf10 00000002 00000002 00000000 cfc29df0
ffa0: c02745e4 cff9cf00 00000013 00000000 00000000 00000000 cf46fff4 cf46ffc8
ffc0: c0063704 c02745f4 00000000 00000000 cf46ffd0 cf46ffd0 00000000 cfc29df0
ffe0: c006367c c004f490 00000000 cf46fff8 c004f490 c006368c 00000000 00000000
Backtrace:
[<c0298f34>] (ubi_leb_read+0x0/0x124) from [<c029f998>] (ubiblock_readsect+0xbc/0xec)
r8:cf21d400 r7:00000400 r6:00000200 r5:00000200 r4:cff9cea0
[<c029f8dc>] (ubiblock_readsect+0x0/0xec) from [<c02747d0>] (mtd_blktrans_thread+0x1ec/0x308)
[<c02745e4>] (mtd_blktrans_thread+0x0/0x308) from [<c0063704>] (kthread+0x88/0x94)
[<c006367c>] (kthread+0x0/0x94) from [<c004f490>] (do_exit+0x0/0x6c0)
r6:c004f490 r5:c006367c r4:cfc29df0
Code: e1a0c00d e92dd9f0 e24cb004 e24dd014 (e5905000)
---[ end trace 764c279107f929b4 ]---
udevd[135]: worker [162] timeout, kill it
udevd[135]: seq 1299 '/devices/virtual/mtd/mtd2/ubiblka' killed
udevd[135]: worker [162] terminated by signal 9 (Killed)
Starting Bootlog daemon:
I'm calling the kernel with this parameters
bootargs_mtd 'setenv bootargs ${bootargs} ubi.mtd=2 root=ubi0_0 rootfstype=ubifs rw init=/sbin/init console=${tty},${baudrate} gpmi'
I'm sending my kernel .config attached
Original Attachment has been moved to: defconfig.ubi.zip
解決済! 解決策の投稿を見る。
Potentially, yes: http://comments.gmane.org/gmane.linux.drivers.mtd/34682
Looks like either going to a new kernel or back-porting the driver seem to be the solution since I can't find a patch for the reported issue.
Hi Guilherme,
I would suggest you to try a 3.13 kernel. If you still see issues with 3.13 then report it to the linux-mtd mailing list.
Regards,
Fabio Estevam
Hi Fabio, I Can not change to kernel 3.13, but is there any know issues with imx28 + kernel 2.6.35 + ubifs?
Thanks
Hi Guilherme,
Usually it is easier to obtain support from the developers in the mtd community when you use a recent kernel. Kernel 2.6.35 is very old right now.
Maybe you could take a look at this nice tutorial about UBIFS on mx28:
FlashFilesystemsUBIFS < DULG < DENX
Regards,
Fabio Estevam
Potentially, yes: http://comments.gmane.org/gmane.linux.drivers.mtd/34682
Looks like either going to a new kernel or back-porting the driver seem to be the solution since I can't find a patch for the reported issue.
Thanks Kursad i made a back-port of the solutuion for my error and think It's working