Imx28 EVK UART pinouts

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Imx28 EVK UART pinouts

572 次查看
jamakh
Contributor I

Hi,

I want to use UART at higher baud rates but I see Maxim transceivers do not support beyond 115200bps. Is there any other way to use UART at higher baud rates?

I see J63 can be used where UART pins are available but from where I can find its connector?

Thanks

Jam

标签 (1)
0 项奖励
1 回复

414 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jam

you are right, also I think you can ask maxim for compatible

more higher rates transceivers and try to resolder that part.

Regarding J63 you can look at complete BOM file (link below)

and obtain mating connector locally or order it from some

stock company (like mouser or farnel).

IMX28_EVK_DESIGN_FILES_R10

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励