Imx-wm8958 Speaker is not switchin ON once headphone is unplugged

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Imx-wm8958 Speaker is not switchin ON once headphone is unplugged

570件の閲覧回数
srikanthmediset
Contributor I

Hi ,

   I am working on Android 6 imx-wm8958 audio driver.Initially without connecting headphone audio output was coming properly from externel speaker.When I insert the head jack audio was comin from head jack properly.Once I remove head jack audio was not coming from externel speaker.That means speaker was not able to revert back to ON state once head p\jack was unplugged.

  Can anyone help me over this.

Regards

srikanth.

ラベル(4)
0 件の賞賛
2 返答(返信)

447件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello

I do not know if you are still having a problem.

If yes, can you please tell me which board and i.MX are you using?

Best Regards,

Diego.

0 件の賞賛

447件の閲覧回数
srikanthmediset
Contributor I

Hi,

  Yes,still I have the issue.I am using iMX6 sabre sd with Android marshmallow running in it.

RegardsSrikanth.

Sent from Yahoo Mail on Android

On Thu, 8 Mar 2018 at 11:35 PM, diegoadrian<admin@community.nxp.com> wrote:

#yiv7371088348 * #yiv7371088348 a #yiv7371088348 body {font-family:Helvetica, Arial, sans-serif;}#yiv7371088348 #yiv7371088348 h1, #yiv7371088348 h2, #yiv7371088348 h3, #yiv7371088348 h4, #yiv7371088348 h5, #yiv7371088348 h6, #yiv7371088348 p, #yiv7371088348 hr {}#yiv7371088348 .yiv7371088348button td {}

|

NXP Community

|

Re: Imx-wm8958 Speaker is not switchin ON once headphone is unplugged

reply from Diego Adrian Cuevas in i.MX Community - View the full discussion

Hello

 

I do not know if you are still having a problem.

 

If yes, can you please tell me which board and i.MX are you using?

 

Best Regards,

Diego.

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in i.MX Community by email or at NXP Community

Following Re: Imx-wm8958 Speaker is not switchin ON once headphone is unplugged in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 件の賞賛