Ilitek ILI9881C MIPI LCD Panel not work on i.MX93

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ilitek ILI9881C MIPI LCD Panel not work on i.MX93

1,389 Views
wenxue_guo
Contributor III

Hi,

I'm debugging our LCD panel based Ilitek ILI9881C on our new i.MX93 board with BSP version LF-6.1.22-2.0.0, it works fine on our some other boards based on i.MX8MN, i.MX8MM, i.MX8MQ, i.MX8ULP.

 

Below is our DTS configuration for MIPI LCD panel:

&dphy {
    status = "okay";
};

&lcdif {
    status = "okay";
    assigned-clock-rates = <282404000>, <70601000>, <400000000>, <133333333>;
};

&dsi{
    status = "okay";
    #address-cells = <1>;
    #size-cells = <0>;

    panel@0 {
        compatible = "avnet,ph720128t003", "ilitek,ili9881c";
        reg = <0>;
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_gpio_backlight>;
        pwn-gpios = <&gpio2 6 GPIO_ACTIVE_HIGH>;
        dsi-lanes = <2>;
        backlight = <&backlight>;

        port {
            panel_in: endpoint {
                remote-endpoint = <&mipi_dsi_out>;
            };  
        };  

    };  

    ports {
        #address-cells = <1>;
        #size-cells = <0>;

        port@1 {
            reg = <1>;
            mipi_dsi_out: endpoint {
            remote-endpoint = <&panel_in>;
            };  
        };  
    };  
};

 

And this our LCD driver configuration, it works fine on all other i.MX8 serial boards.

static const struct drm_display_mode ph720128t003_default_mode = {

    .clock      = 70601, /* htotal*vtotal*fps = 900x1307x60.02= 70,601,526 */

    .hdisplay   = 720, 
    .hsync_start= 720 + 120, 
    .hsync_end  = 720 + 120 + 40,
    .htotal     = 720 + 120 + 40 + 20,

    .vdisplay   = 1280,
    .vsync_start= 1280 + 10,
    .vsync_end  = 1280 + 10 + 2, 
    .vtotal     = 1280 + 10 + 2 + 15,

    .width_mm   = 153, 
    .height_mm  = 90,
};

 

But it can not work on I.MX93 board.

Notwork.jpg

 

I try to modify the assigned-clock-rates value in &lcdif in the DTS file, but there is no effect whatsoever. Then I try to change pix clock in the LCD panel driver, and found it can work on 72.6MHz (Not 70.601MHz) with some bugs.

static const struct drm_display_mode ph720128t003_default_mode = {

    .clock      = 72600, /* htotal*vtotal*fps = 900x1307x60.02= 70,601,526 */

    .hdisplay   = 720, 
    .hsync_start= 720 + 120, 
    .hsync_end  = 720 + 120 + 40,
    .htotal     = 720 + 120 + 40 + 20,

    .vdisplay   = 1280,
    .vsync_start= 1280 + 10,
    .vsync_end  = 1280 + 10 + 2, 
    .vtotal     = 1280 + 10 + 2 + 15,

    .width_mm   = 153, 
    .height_mm  = 90,
};

 

Below is the LCD display result when I execute "modetest -M imx-drm -D 1 -a -s 35@33:720x1280 -P 31@33:720x1280" for some times.

ModeBlue.jpgModeGreen.jpgModeRed.jpg

 

Now the problem is:

1,  The RGB color will change when I execute command "modetest -M imx-drm -D 1 -a -s 35@33:720x1280 -P 31@33:720x1280" every time;

2, Some pixels will overflow from bottom/right to top/left, and can not be fixed by change the value of  HSPW/HFP/HBP/VSPW/VFP/VBP;

 

So my question is how to configure the MIPI-DSI clock for our custom panel, and can anyone give me some guide to fix this bug? Thanks in advanced! 

0 Kudos
11 Replies

1,099 Views
leevi_li
Contributor I

Hi, I'm Wenxue_Guo's colleague. 

We have determined the LCD parameters through the original factory.  Now it has been set, and the clock has been set according to the method provided above, but it is still not correct.  The following is some information I modified and the picture is attached.  Now there may be some problems, how should we check?  Please take a look, Thanks a lot!

 

The following is the lcd parameters we want to find the manufacturer:图片1.png

 

Here are my code changes:

图片2.png

 

Gets the clock after recompiling:

图片3.png

 

Using fb-test to test the screen, the screen does not display properly:

IMG_20240131_181825.jpg

 

0 Kudos

1,057 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @leevi_li 

I have another idea,  please keep timing as before and dump MIPI DSI and DPHY registers.

0 Kudos

1,041 Views
leevi_li
Contributor I

Hi, @Zhiming_Liu 

 

I have dumped the MIPI DSI and DPHY registers, and restore the previous lcd configuration parameters. Here are my changes and the results:

 

I added a function to the dw_mipi_dsi_host_transfer function that prints the register as follows:

leevi_li_0-1706782837247.png

Added dump_MIPI_DSI_and_DPHY_registers()  functions:

520	static void  dump_MIPI_DSI_and_DPHY_registers(struct dw_mipi_dsi *dsi)
521	{
522		u32 address = 0;
523		u32 val = 0;
524
525		printk("[%s.%d],\n\n", __FUNCTION__,__LINE__);
526
527		address = DSI_VERSION;
528		val = dsi_read(dsi, address);
529		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
530
531		address = DSI_PWR_UP;
532		val = dsi_read(dsi, address);
533		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
534
535		address = DSI_CLKMGR_CFG;
536		val = dsi_read(dsi, address);
537		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
538
539		address = DSI_DPI_VCID;
540		val = dsi_read(dsi, address);
541		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
542
543		address = DSI_DPI_COLOR_CODING;
544		val = dsi_read(dsi, address);
545		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
546
547		address = DSI_DPI_CFG_POL;
548		val = dsi_read(dsi, address);
549		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
550
551		address = DSI_DPI_LP_CMD_TIM;
552		val = dsi_read(dsi, address);
553		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
554
555		address = DSI_DBI_VCID;
556		val = dsi_read(dsi, address);
557		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
558
559		address = DSI_DBI_CFG;
560		val = dsi_read(dsi, address);
561		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
562
563		address = DSI_DBI_PARTITIONING_EN;
564		val = dsi_read(dsi, address);
565		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
566
567		address = DSI_DBI_CMDSIZE;
568		val = dsi_read(dsi, address);
569		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
570
571		address = DSI_PCKHDL_CFG;
572		val = dsi_read(dsi, address);
573		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
574
575		address = DSI_GEN_VCID;
576		val = dsi_read(dsi, address);
577		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
578
579		address = DSI_MODE_CFG;
580		val = dsi_read(dsi, address);
581		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
582
583		address = DSI_VID_MODE_CFG;
584		val = dsi_read(dsi, address);
585		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
586
587		address = DSI_VID_PKT_SIZE;
588		val = dsi_read(dsi, address);
589		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
590
591		address = DSI_VID_NUM_CHUNKS;
592		val = dsi_read(dsi, address);
593		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
594
595		address = DSI_VID_NULL_SIZE;
596		val = dsi_read(dsi, address);
597		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
598
599		address = DSI_VID_HSA_TIME;
600		val = dsi_read(dsi, address);
601		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
602
603		address = DSI_VID_HBP_TIME;
604		val = dsi_read(dsi, address);
605		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
606
607		address = DSI_VID_HLINE_TIME;
608		val = dsi_read(dsi, address);
609		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
610
611		address = DSI_VID_VSA_LINES;
612		val = dsi_read(dsi, address);
613		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
614
615		address = DSI_VID_VBP_LINES;
616		val = dsi_read(dsi, address);
617		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
618
619		address = DSI_VID_VFP_LINES;
620		val = dsi_read(dsi, address);
621		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
622
623		address = DSI_VID_VACTIVE_LINES;
624		val = dsi_read(dsi, address);
625		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
626
627		address = DSI_EDPI_CMD_SIZE;
628		val = dsi_read(dsi, address);
629		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
630
631		address = DSI_CMD_MODE_CFG;
632		val = dsi_read(dsi, address);
633		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
634
635		address = DSI_GEN_HDR;
636		val = dsi_read(dsi, address);
637		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
638
639		address = DSI_GEN_PLD_DATA;
640		val = dsi_read(dsi, address);
641		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
642
643		address = DSI_CMD_PKT_STATUS;
644		val = dsi_read(dsi, address);
645		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
646
647		address = DSI_TO_CNT_CFG;
648		val = dsi_read(dsi, address);
649		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
650
651		address = DSI_HS_RD_TO_CNT;
652		val = dsi_read(dsi, address);
653		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
654
655		address = DSI_LP_RD_TO_CNT;
656		val = dsi_read(dsi, address);
657		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
658
659		address = DSI_HS_WR_TO_CNT;
660		val = dsi_read(dsi, address);
661		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
662
663		address = DSI_LP_WR_TO_CNT;
664		val = dsi_read(dsi, address);
665		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
666
667		address = DSI_BTA_TO_CNT;
668		val = dsi_read(dsi, address);
669		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
670
671		address = DSI_LPCLK_CTRL;
672		val = dsi_read(dsi, address);
673		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
674
675		address = DSI_PHY_TMR_LPCLK_CFG;
676		val = dsi_read(dsi, address);
677		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
678
679		address = DSI_PHY_TMR_CFG;
680		val = dsi_read(dsi, address);
681		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
682
683		address = DSI_PHY_RSTZ;
684		val = dsi_read(dsi, address);
685		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
686
687		address = DSI_PHY_IF_CFG;
688		val = dsi_read(dsi, address);
689		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
690
691		address = DSI_PHY_ULPS_CTRL;
692		val = dsi_read(dsi, address);
693		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
694
695		address = DSI_PHY_TX_TRIGGERS;
696		val = dsi_read(dsi, address);
697		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
698
699		address = DSI_PHY_STATUS;
700		val = dsi_read(dsi, address);
701		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
702
703		address = DSI_PHY_TST_CTRL0;
704		val = dsi_read(dsi, address);
705		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
706
707		address = DSI_PHY_TST_CTRL1;
708		val = dsi_read(dsi, address);
709		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
710
711		address = DSI_INT_ST0;
712		val = dsi_read(dsi, address);
713		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
714
715		address = DSI_INT_ST1;
716		val = dsi_read(dsi, address);
717		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
718
719		address = DSI_INT_MSK0;
720		val = dsi_read(dsi, address);
721		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
722
723		address = DSI_INT_MSK1;
724		val = dsi_read(dsi, address);
725		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
726
727		address = DSI_PHY_TMR_RD_CFG;
728		val = dsi_read(dsi, address);
729		printk("[%s.%d], address=0x%x, val=0x%x\n", __FUNCTION__,__LINE__, address, val);
730
731	}

 

The final printed result is as follows:

[ 1723.823656] [dw_mipi_dsi_host_transfer.742],
[ 1723.823656] 
[ 1723.831052] [dump_MIPI_DSI_and_DPHY_registers.525],
[ 1723.831052] 
[ 1723.839049] [dump_MIPI_DSI_and_DPHY_registers.529], address=0x0, val=0x3134312a
[ 1723.847252] [dump_MIPI_DSI_and_DPHY_registers.533], address=0x4, val=0x1
[ 1723.854839] [dump_MIPI_DSI_and_DPHY_registers.537], address=0x8, val=0x6
[ 1723.862551] [dump_MIPI_DSI_and_DPHY_registers.541], address=0xc, val=0x0
[ 1723.870157] [dump_MIPI_DSI_and_DPHY_registers.545], address=0x10, val=0x5
[ 1723.877835] [dump_MIPI_DSI_and_DPHY_registers.549], address=0x14, val=0x0
[ 1723.885515] [dump_MIPI_DSI_and_DPHY_registers.553], address=0x18, val=0x100004
[ 1723.893612] [dump_MIPI_DSI_and_DPHY_registers.557], address=0x1c, val=0x0
[ 1723.901279] [dump_MIPI_DSI_and_DPHY_registers.561], address=0x20, val=0x0
[ 1723.908989] [dump_MIPI_DSI_and_DPHY_registers.565], address=0x24, val=0x0
[ 1723.916678] [dump_MIPI_DSI_and_DPHY_registers.569], address=0x28, val=0x0
[ 1723.924370] [dump_MIPI_DSI_and_DPHY_registers.573], address=0x2c, val=0x1c
[ 1723.932137] [dump_MIPI_DSI_and_DPHY_registers.577], address=0x30, val=0x0
[ 1723.939916] [dump_MIPI_DSI_and_DPHY_registers.581], address=0x34, val=0x0
[ 1723.947605] [dump_MIPI_DSI_and_DPHY_registers.585], address=0x38, val=0xbf00
[ 1723.955530] [dump_MIPI_DSI_and_DPHY_registers.589], address=0x3c, val=0x2d0
[ 1723.963365] [dump_MIPI_DSI_and_DPHY_registers.593], address=0x40, val=0x0
[ 1723.971024] [dump_MIPI_DSI_and_DPHY_registers.597], address=0x44, val=0x0
[ 1723.978688] [dump_MIPI_DSI_and_DPHY_registers.601], address=0x48, val=0x3c
[ 1723.986443] [dump_MIPI_DSI_and_DPHY_registers.605], address=0x4c, val=0x1e
[ 1723.994200] [dump_MIPI_DSI_and_DPHY_registers.609], address=0x50, val=0x546
[ 1724.002005] [dump_MIPI_DSI_and_DPHY_registers.613], address=0x54, val=0x2
[ 1724.009646] [dump_MIPI_DSI_and_DPHY_registers.617], address=0x58, val=0xf
[ 1724.017251] [dump_MIPI_DSI_and_DPHY_registers.621], address=0x5c, val=0xa
[ 1724.024846] [dump_MIPI_DSI_and_DPHY_registers.625], address=0x60, val=0x500
[ 1724.032584] [dump_MIPI_DSI_and_DPHY_registers.629], address=0x64, val=0x0
[ 1724.040152] [dump_MIPI_DSI_and_DPHY_registers.633], address=0x68, val=0x10f7f00
[ 1724.048247] [dump_MIPI_DSI_and_DPHY_registers.637], address=0x6c, val=0x2905
[ 1724.056082] [dump_MIPI_DSI_and_DPHY_registers.641], address=0x70, val=0x0
[ 1724.063645] [dump_MIPI_DSI_and_DPHY_registers.645], address=0x74, val=0x50015
[ 1724.071586] [dump_MIPI_DSI_and_DPHY_registers.649], address=0x78, val=0x3e803e8
[ 1724.079679] [dump_MIPI_DSI_and_DPHY_registers.653], address=0x7c, val=0x0
[ 1724.087260] [dump_MIPI_DSI_and_DPHY_registers.657], address=0x80, val=0x0
[ 1724.094955] [dump_MIPI_DSI_and_DPHY_registers.661], address=0x84, val=0x0
[ 1724.102567] [dump_MIPI_DSI_and_DPHY_registers.665], address=0x88, val=0x0
[ 1724.110277] [dump_MIPI_DSI_and_DPHY_registers.669], address=0x8c, val=0xd00
[ 1724.118049] [dump_MIPI_DSI_and_DPHY_registers.673], address=0x94, val=0x1
[ 1724.125635] [dump_MIPI_DSI_and_DPHY_registers.677], address=0x98, val=0x3a0073
[ 1724.133657] [dump_MIPI_DSI_and_DPHY_registers.681], address=0x9c, val=0x230058
[ 1724.141676] [dump_MIPI_DSI_and_DPHY_registers.685], address=0xa0, val=0xf
[ 1724.149329] [dump_MIPI_DSI_and_DPHY_registers.689], address=0xa4, val=0x2001
[ 1724.157188] [dump_MIPI_DSI_and_DPHY_registers.693], address=0xa8, val=0x0
[ 1724.164766] [dump_MIPI_DSI_and_DPHY_registers.697], address=0xac, val=0x0
[ 1724.172346] [dump_MIPI_DSI_and_DPHY_registers.701], address=0xb0, val=0x1529
[ 1724.180323] [dump_MIPI_DSI_and_DPHY_registers.705], address=0xb4, val=0x0
[ 1724.187939] [dump_MIPI_DSI_and_DPHY_registers.709], address=0xb8, val=0x0
[ 1724.195545] [dump_MIPI_DSI_and_DPHY_registers.713], address=0xbc, val=0x0
[ 1724.203132] [dump_MIPI_DSI_and_DPHY_registers.717], address=0xc0, val=0x800
[ 1724.210893] [dump_MIPI_DSI_and_DPHY_registers.721], address=0xc4, val=0x0
[ 1724.218477] [dump_MIPI_DSI_and_DPHY_registers.725], address=0xc8, val=0x0
[ 1724.226060] [dump_MIPI_DSI_and_DPHY_registers.729], address=0xf4, val=0x2710

 

My lcd parameters remain the same as before, but the clock has been fixed:

leevi_li_1-1706783316283.png

 

static const struct drm_display_mode ph720128t005_default_mode = {
	.clock		= 70500,    // clock = 900 * 1307 * 60.02fps = 70601526

	.hdisplay	= 720,
	.hsync_start= 720 + 120,
	.hsync_end	= 720 + 120 + 40,
	.htotal		= 720 + 120 + 40 + 20,

	.vdisplay	= 1280,
	.vsync_start= 1280 + 10,
	.vsync_end	= 1280 + 10 + 2,
	.vtotal		= 1280 + 10 + 2 + 15,

	.width_mm	= 155,
	.height_mm	= 87,
};

 Gets the clock after recompiling:

leevi_li_2-1706783540989.png

After this modification, I was surprised to find that the screen seemed to display normally,

Below is the display of fb-test and the startup screen:

IMG_20240201_183351.jpgIMG_20240201_183301.jpg

 

As for the modification, I checked it and finally found that it was affected by the added printing. I removed the printing in the dw_mipi_dsi_host_transfer function, and the test result returned to the previous state, as shown in the figure below,:

 

Now the question is, why is printing added to the dw_mipi_dsi_host_transfer function, so there are different results, please help analyze it, Thanks a lot.

 

IMG_20240201_142823.jpgIMG_20240201_142907.jpg

0 Kudos

1,032 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @leevi_li 

 

The data sync may have issue for the dsi default setting, you can refer below photo, the current frame exists previous frame. This is root cause. As @guowen_xue said, this panel works on i.MX8 series, and i.MX93 is using DWC DSI IP, so the default DSI setting except timing may be different. You added the log print causes the transfer delay and then this delay fixup the sync issue.

 

Zhiming_Liu_0-1706846395116.png

 

Here is sync settings in DSI driver 

static void dw_mipi_dsi_video_mode_config(struct dw_mipi_dsi *dsi)
{
	u32 val;

	/*
	 * TODO dw drv improvements
	 * enabling low power is panel-dependent, we should use the
	 * panel configuration here...
	 */
	val = ENABLE_LOW_POWER;

	if (dsi->mode_flags & MIPI_DSI_MODE_VIDEO_BURST)
		val |= VID_MODE_TYPE_BURST;
	else if (dsi->mode_flags & MIPI_DSI_MODE_VIDEO_SYNC_PULSE)
		val |= VID_MODE_TYPE_NON_BURST_SYNC_PULSES;
	else
		val |= VID_MODE_TYPE_NON_BURST_SYNC_EVENTS;

#ifdef CONFIG_DEBUG_FS
	if (dsi->vpg_defs.vpg) {
		val |= VID_MODE_VPG_ENABLE;
		val |= dsi->vpg_defs.vpg_horizontal ?
		       VID_MODE_VPG_HORIZONTAL : 0;
		val |= dsi->vpg_defs.vpg_ber_pattern ? VID_MODE_VPG_MODE : 0;
	}
#endif /* CONFIG_DEBUG_FS */

	dsi_write(dsi, DSI_VID_MODE_CFG, val);
}

static void dw_mipi_dsi_set_mode(struct dw_mipi_dsi *dsi,
				 unsigned long mode_flags)
{
	u32 val;

	dsi_write(dsi, DSI_PWR_UP, RESET);

	if (mode_flags & MIPI_DSI_MODE_VIDEO) {
		dsi_write(dsi, DSI_MODE_CFG, ENABLE_VIDEO_MODE);
		dw_mipi_dsi_video_mode_config(dsi);
	} else {
		dsi_write(dsi, DSI_MODE_CFG, ENABLE_CMD_MODE);
	}

	val = PHY_TXREQUESTCLKHS;
	if (dsi->mode_flags & MIPI_DSI_CLOCK_NON_CONTINUOUS)
		val |= AUTO_CLKLANE_CTRL;
	dsi_write(dsi, DSI_LPCLK_CTRL, val);

	dsi_write(dsi, DSI_PWR_UP, POWERUP);
}

static void dw_mipi_dsi_dpi_config(struct dw_mipi_dsi *dsi,
				   const struct drm_display_mode *mode)
{
	u32 val = 0, color = 0;

	switch (dsi->format) {
	case MIPI_DSI_FMT_RGB888:
		color = DPI_COLOR_CODING_24BIT;
		break;
	case MIPI_DSI_FMT_RGB666:
		color = DPI_COLOR_CODING_18BIT_2 | LOOSELY18_EN;
		break;
	case MIPI_DSI_FMT_RGB666_PACKED:
		color = DPI_COLOR_CODING_18BIT_1;
		break;
	case MIPI_DSI_FMT_RGB565:
		color = DPI_COLOR_CODING_16BIT_1;
		break;
	}

	if (mode->flags & DRM_MODE_FLAG_NVSYNC)
		val |= VSYNC_ACTIVE_LOW;
	if (mode->flags & DRM_MODE_FLAG_NHSYNC)
		val |= HSYNC_ACTIVE_LOW;

	dsi_write(dsi, DSI_DPI_VCID, DPI_VCID(dsi->channel));
	dsi_write(dsi, DSI_DPI_COLOR_CODING, color);
	dsi_write(dsi, DSI_DPI_CFG_POL, val);
}

 

You need confirm what's type of sync about your panel and add these sync flags into the panel-simple.c

Usable flags:

MIPI_DSI_MODE_VIDEO_SYNC_PULSE
MIPI_DSI_MODE_VIDEO_BURST
DRM_MODE_FLAG_NVSYNC
DRM_MODE_FLAG_NHSYNC
 
You can refer this drivers/gpu/drm/panel/panel-ilitek-ili9881c.c
Zhiming_Liu_1-1706846986345.png

 

 
And then modify the drm_display_mode like blow structure, add DRM_MODE_FLAG in drm_display_mode and MIPI_DSI_MODE in panel_desc_dsi.
 
static const struct drm_display_mode boe_tv080wum_nl0_mode = {
	.clock = 160000,
	.hdisplay = 1200,
	.hsync_start = 1200 + 120,
	.hsync_end = 1200 + 120 + 20,
	.htotal = 1200 + 120 + 20 + 21,
	.vdisplay = 1920,
	.vsync_start = 1920 + 21,
	.vsync_end = 1920 + 21 + 3,
	.vtotal = 1920 + 21 + 3 + 18,
	.flags = DRM_MODE_FLAG_NVSYNC | DRM_MODE_FLAG_NHSYNC,
};

static const struct panel_desc_dsi boe_tv080wum_nl0 = {
	.desc = {
		.modes = &boe_tv080wum_nl0_mode,
		.num_modes = 1,
		.size = {
			.width = 107,
			.height = 172,
		},
		.connector_type = DRM_MODE_CONNECTOR_DSI,
	},
	.flags = MIPI_DSI_MODE_VIDEO |
		 MIPI_DSI_MODE_VIDEO_BURST |
		 MIPI_DSI_MODE_VIDEO_SYNC_PULSE,
	.format = MIPI_DSI_FMT_RGB888,
	.lanes = 4,
};

 

 

0 Kudos

984 Views
leevi_li
Contributor I

Hi, @Zhiming_Liu 

You mean, there's still something wrong with the sync signal. We still have to fix the sync signal error?

At present, I first handled this problem according to the delay, and replaced the previous printing with a delay. Currently, both screens in the test are normal. After I added the delay, all the changes are as follows:

leevi_li_4-1707041847447.png

leevi_li_5-1707041905774.png

leevi_li_6-1707041923069.png

 

Now, I follow the changes you provided, but there are compilation problems. Below are my modifications, and the compilation error messages printed

leevi_li_8-1707042981373.png

 

leevi_li_0-1707041445037.png

leevi_li_1-1707041502894.pngleevi_li_2-1707041526174.png

At the same time, I have a question, this added struct, how does it get called?

leevi_li_7-1707042458558.png

 

Attached is the complete file panel-ilitek-ili9881c.c

 

Thanks a lot!

0 Kudos

1,368 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You need modify drivers/clk/imx/clk-fracn-gppll.c to support new pixel clock

 

Please refer 74.2.3 Clock configuration in RM.

If we add a frequency of 537.6MHz(Pixel clock *4), then MFI=112, MFN=0, MFD=1, rdiv=0, odiv=5
The root source of VIDEO_PLL is Fref = 24M, then Fvco = Fref * (MFI + MFN / MFD)=2688

Then Fout = Fvco / (rdiv * odiv)= 537.6

Zhiming_Liu_0-1704855409879.png

Configure new pixel clock 134.4MHz and VIDEO_PLL to LCDIF in dts:

Zhiming_Liu_1-1704855424686.png

 

0 Kudos

1,363 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You can try below value:

mfi: 141

mfn: 1

mfd: 5

rdiv: 1

odiv: 12

0 Kudos

1,355 Views
wenxue_guo
Contributor III

Hi @Zhiming_Liu ,

Thanks for your reply! After do the modify as your guide, the LCD panel still get same bugs.

patch.png

 

The clock seems changed.

 

root@maaxboardosm93:~# cat /sys/kernel/debug/clk/media_disp_pix_root/clk_rate 
70600000

 

 

But the RGB color still changes when execute modetest command, and the first pixel coordinates is wrong now.

lcd.jpg

 

Can you give me some other clue?

 

By the way, My Reference Manual is Rev. 1, 10/2022, there is no 74.2.3 Clock configuration in this document. I'm a bit confused about this formula:

Fvco = Fref * (MFI + MFN / MFD)

Fout = Fvco / (rdiv * odiv)

 

Take these configuration in the source code as example:

 

PLL_FRACN_GP(1700000000U, 141, 0, 0, 1, 2),

Fvco = Fref * (MFI + MFN / MFD)=24*(141+0/0) ?

 

PLL_FRACN_GP(300000000U, 150, 0, 1, 0, 12)

Fvco = Fref * (MFI + MFN / MFD)=24*(150+0/1) = 3600

Fout = Fvco / (rdiv * odiv)= 3600 / ( 0*12 )  ??

 

Thanks a lot!

 

 

0 Kudos

1,351 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

For the issue in photo , you need set output section in /etc/xdg/weston/weston.ini. 

Add your panel information and rotate.  Can you confirm that your timing is correct?

 

For mfd, rdiv and odiv, if they are zero, the hardware will treat them as 1.

0 Kudos

1,347 Views
wenxue_guo
Contributor III

Hi @Zhiming_Liu ,

1, It's not for the weston configuration, because the linux penguin logo Tux display on the wrong position too when kernel boot up, and libdrm test command modetest get the same result.

2, This LCD panel timing can work fine on our i.MX8MN, i.MX8MM, i.MX8MQ, i.MX8ULP boards, and I'll confirm with our LCD panel provider.

3, Yep, the div bit set be 0 always treat them as 1(Fout=Fin/(div+1)). Then how does set it be 1 for mfd, rdiv and odiv? Does the hardware treat them as 1 or 2, and the value in formula should be 1 or 2?

 

Thanks a lot!

0 Kudos

1,343 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

If mfd, rdiv, odiv equals 1, they are still 1. The zero is special case.

0 Kudos