Does the NVCC_xxx supply can be combined with VDD_HIGH_IN and VDD_SNVS_IN in IMX6ULL design?
Hi Vadim
this is not allowed as datasheet sect.4.2.1 Power-Up Sequence requires
VDD_SNVS_IN supply to be turned on before any other power supply.
i.MX 6ULL Applications Processors for Consumer Products
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI Igor,
Is there any reason why it differs from the i.MX6UL where both supplies can be tight together?
br,
Rod
Hi Rod
>Is there any reason why it differs from the i.MX6UL where both supplies can be tight together?
I thnk it has similar design as i.MX6UL and the same power-up sequence.
Best regardsThen which one is right? 6UL or 6ULL?
And then we have to correct the Datasheet
Br,
Rod
Hi Rod
I think both are right.
Best regards
igor