If iMX8M with DDR3L design,the platform need to patch bl31.bin?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

If iMX8M with DDR3L design,the platform need to patch bl31.bin?

Jump to solution
1,186 Views
felixhsu
Contributor III

Hi All

The community had release for LPDDR4 bl31.bin patch, if customer use DDR3L design platform, the platform need to patch bl31.bin or not?

https://community.nxp.com/docs/DOC-340179 

Thanks.

Labels (2)
0 Kudos
Reply
1 Solution
762 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Generally the Arm trusted firmware BL31 should not depend on memory type.

The patch is intended for DVFS and will work only with same type memories as our EVK.


Look at the following:

imx8mq GA release: DDR initialization in ATF 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
763 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Generally the Arm trusted firmware BL31 should not depend on memory type.

The patch is intended for DVFS and will work only with same type memories as our EVK.


Look at the following:

imx8mq GA release: DDR initialization in ATF 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply