IPU1 and IPU2 Addresses

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IPU1 and IPU2 Addresses

Jump to solution
822 Views
christianbach
Contributor I

i.MX 6Dual/6Quad

The file soc_memory_map.h shows the following addresses

#define IPU1_ARB_BASE_ADDR   0x02400000
#define IPU1_ARB_END_ADDR   0x027FFFFF
#define IPU2_ARB_BASE_ADDR   0x02800000
#define IPU2_ARB_END_ADDR   0x02BFFFFF

but Table 2-1 in the reference manual shows the following:

Start addressEnd addressSizeDescription

02A0_0000

02DF_FFFF4 MBIPU-2
0260_0000029F_FFFF4 MBIPU-1

which address is correct?

Labels (1)
0 Kudos
Reply
1 Solution
708 Views
igorpadykov
NXP Employee
NXP Employee

Hi Christian

both correct, SDK except soc_memory_map.h, also adds below value

for IPU address calculation defined in ipu_reg_def.h

#define IPU_REGISTERS_OFFSET   0x00200000

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
709 Views
igorpadykov
NXP Employee
NXP Employee

Hi Christian

both correct, SDK except soc_memory_map.h, also adds below value

for IPU address calculation defined in ipu_reg_def.h

#define IPU_REGISTERS_OFFSET   0x00200000

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply