IPU's in imx8M-Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IPU's in imx8M-Mini

1,784 Views
sumankumar
Contributor I

Hi,

How many IPU's does the imx8m-MINI support.

I see imx8m-mini has ONE CSI controller.

Our present system uses two mipi cameras(13MP and 5MP) and a parallel fingerprint device on imx6.

Best,

Suman

0 Kudos
7 Replies

1,360 Views
sumankumar
Contributor I

Thanks igorpadykov.

Does i.MX8M-Mini support TWO IPU's?

I went through the Processor Spec (IMX8MMRM.pdf) but could not find details about IPUs.

For imx6, i get them in an application note

https://www.nxp.com/docs/en/application-note/AN5305.pdf

Do you have something similar for imx8Mmini?

Best,

Suman

0 Kudos

1,360 Views
igorpadykov
NXP Employee
NXP Employee

Hi Suman

i.MX8M-Mini has not IPU modules, it is completely different than i.MX6 processor.

Best regards
igor

0 Kudos

1,360 Views
sumankumar
Contributor I

Hi igorpadykov,

Can you point me to the reference docs to understand more about internals of CSI blocks on imx8M-mini?

Our present system on imx6 has 3 peripherals.

1. Parallel 0 -> mapped to a parallel finger print sensor

2. Virtual Channel 1 (VC1) mapped to CSI1 of IPU1

3. VC2 mapped to CSI0 of IPU2.

We are evaluating to move to iMX8M-Mini. What are the technically feasible options to have the above functionalities on i.MX8M-Mini 

0 Kudos

1,360 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos

1,360 Views
sumankumar
Contributor I

Thanks Igor. I went through Chapter 13, section CSI Bridge and MIPI CSI Host Controller of the said document.

Since there are no IPUs, What is your recommendation for design to have all 3 peripherals?

1. Parallel FingerPrint

2. TWO mipi csi cameras.

Best,

Suman

0 Kudos

1,360 Views
igorpadykov
NXP Employee
NXP Employee

Hi Suman

for two mipi csi cameras better to use i.MX8M, it has two mipi csi modules.

There is no parallel interface support in i.MX8M (Mini), one can consider i2c/spi/uart to

parallel converter, probably with fpga.

Best regards
igor

0 Kudos

1,360 Views
igorpadykov
NXP Employee
NXP Employee

Hi Suman

correct, i.MX8M Mini has one MIPI-CSI module, as described in

AN12296 i.MX 8M Mini Migration Guide

https://www.nxp.com/docs/en/application-note/AN12296.pdf 

i.MX 8M Mini Applications Processor | Arm Cortex A53/M4 | 1080P display | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos