IOMUX Configuration For IPU1 in IMX6DQ

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IOMUX Configuration For IPU1 in IMX6DQ

586 次查看
ajmalali
Contributor III

Hi,

I am doing some bare-metal programming in iMX6DQ SABRE-SD board. I am using UART1 as the debug serial port. While configuring my UART i have set the Pad Mux Register(IOMUXC_SW_MUX_CTL_PAD_CSI0_DATA10) mux mode field as "011". However, When i try to configure the IPU1 for the device, i have the set the mux mode as "000", as i have observed from the "1.1.0_iMX6_Platform_SDK".

Is it possible to use both these modules simultaneously? 

or should i go for IPU2?

I have never worked with IPU at this level before. Please Help.

Regards,

Ajmal

标签 (4)
0 项奖励
回复
1 回复

450 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ajmal

unfortunately there is no way to use simultaneously gpio and lcd(ipu),

so it is necessary to reassign signal to other pad.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复