[IMXRT685-AUD-EVK] No audio output when building SDK examples with Xtensa Xplorer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[IMXRT685-AUD-EVK] No audio output when building SDK examples with Xtensa Xplorer

280 次查看
fabiosgt
Contributor I

Hi,

I'm trying to build the example dsp_audio_demo_bm_hifi4.
This demo works fine when the flag DSP_IMAGE_COPY_TO_RAM is set to 1, (and the pre-built binaries for dsp are used).
However, there is no audio output when the HiFi 4 binaries are compiled and downloaded to DSP via Xtensa Xplorer and the flag DSP_IMAGE_COPY_TO_RAM is set to 0. No errors are reported on the logs.

Does anyone experience this issue? Are there any differences between the pre-built binaries and the ones I build using the code provided in the example?

 

Thanks in advance,

Fabio

 

标记 (1)
0 回复数