IMXRT1176 SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1176 SDRAM

263 Views
Chethanbg
Contributor III

Hi,

We are developing Instrument cluster application for one of our client using RT1176 controller.

We interfaced Winbond SDRAM 8MB (W9864G6KH-6I).We designed PCB and doing board bringup activity.

Below 2 pins are interchanged

From MCU bank select BA0 is connected to SDRAM BA1

From MCU bank select BA1 is connected to SDRAM BA0

This will cause any issue in SDRAM configuration??if it is causing what configuration settings we should change in firmware?

 

Attached is the image of SDRAM sch

 

 

 

 

0 Kudos
Reply
2 Replies

229 Views
Chethanbg
Contributor III

Any update on above ticket raised?

0 Kudos
Reply

209 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @Chethanbg ,

This is a tough question. We haven't such experience. But I have to say I can't find any reason to oppose it.

 

regards,

Jing

0 Kudos
Reply