IMX8QM hardware design LPDDR4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QM hardware design LPDDR4

Jump to solution
1,735 Views
timur_kh
Contributor II

Hello everyone!
The schematic of IMX8QM (SPF-29420_C5) on pages 14-15 shows an example of an LPDDR4 connection. Do I understand correctly that the DDR_CH[1:0].DQ_[15:0] and DR_CH[1:0].DQ_[31:16] ports can be connected depending on the footprint (simplify PCB design)? If Yes, then this is configure in the Config Tools for i.MX v8?

Second question. In the diagram on page 15, the names of the LPDDR4 channels do not match, i.e. the MX8QP channel A is connected to the LPDDR4 channel B and vice versa, this is also done to simplify the design of the PCB?

Third question. In my device there is DR_CS 1_CS 0_A, but there is no DDR_CH1_CH1_A. How do I properly connect DDR_CS1_CS0_A?

0 Kudos
Reply
1 Solution
1,728 Views
igorpadykov
NXP Employee
NXP Employee

Hi timur_kh

 

> Do I understand correctly that the DDR_CH[1:0].DQ_[15:0] and DR_CH[1:0].DQ_[31:16] ports

>can be connected depending on the footprint (simplify PCB design)?

 

yes

 

>Second question. In the diagram on page 15, the names of the LPDDR4 channels do not match, i.e. the >MX8QP channel A is connected to the LPDDR4 channel B and vice versa, this is also done to simplify the >design of the PCB?

 

yes

 

>Third question. In my device there is DR_CS 1_CS 0_A, but there is no DDR_CH1_CH1_A.

>How do I properly connect DDR_CS1_CS0_A?

 

what do you mean exactly, in SPF-29420_C5 there is also no DDR_CH1_CH1_A.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
3 Replies
1,724 Views
timur_kh
Contributor II

Oh, I made a typo.
Please look at the attached picture.

0 Kudos
Reply
1,711 Views
igorpadykov
NXP Employee
NXP Employee

so what ddr part used in the case, in general in each lpddr4 datasheet section

"Package Block Diagrams" one can find recommended connections.

So if there are no CKE1, CS1 seems this is single rank part, use only CKE0, CS0.

 

Best regards
igor

 

0 Kudos
Reply
1,729 Views
igorpadykov
NXP Employee
NXP Employee

Hi timur_kh

 

> Do I understand correctly that the DDR_CH[1:0].DQ_[15:0] and DR_CH[1:0].DQ_[31:16] ports

>can be connected depending on the footprint (simplify PCB design)?

 

yes

 

>Second question. In the diagram on page 15, the names of the LPDDR4 channels do not match, i.e. the >MX8QP channel A is connected to the LPDDR4 channel B and vice versa, this is also done to simplify the >design of the PCB?

 

yes

 

>Third question. In my device there is DR_CS 1_CS 0_A, but there is no DDR_CH1_CH1_A.

>How do I properly connect DDR_CS1_CS0_A?

 

what do you mean exactly, in SPF-29420_C5 there is also no DDR_CH1_CH1_A.

 

Best regards
igor

0 Kudos
Reply