IMX8QM SCFW CLOCK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8QM SCFW CLOCK

626 次查看
dhty2015
Contributor II

我使用imx8qmmek的板子,从csfw 1.2升级到scfw 1.4。可以运行起来,但是启动android后发现audio相关的时钟都无法使用了,请问scfw相关时钟配置时源码可见的吗,或者适配时钟初始化?

audio_pll1_div 0 0 0 0 0
audio_pll1_clk 0 0 0 0 0
aud_acm_aud_rec_clk1_div 0 0 0 0 0
aud_acm_aud_rec_clk1_clk 0 0 0 0 0
aud_acm_aud_pll_clk1_div 0 0 0 0 0
aud_acm_aud_pll_clk1_clk 0 0 0 0 0
acm_esai0_mclk_sel 0 0 0 0 0
aud_esai0_extal_ipg_clk 0 0 0 0 0
acm_sai7_mclk_sel 0 0 0 0 0
aud_sai7_mclk_clk 0 0 0 0 0
acm_sai6_mclk_sel 0 0 0 0 0
aud_sai6_mclk_clk 0 0 0 0 0
audio_pll0_div 0 0 0 0 0
audio_pll0_clk 0 0 0 0 0
aud_acm_aud_rec_clk0_div 0 0 0 0 0
aud_acm_aud_rec_clk0_clk 0 0 0 0 0
acm_mclkout1_sel 0 0 0 0 0
aud_mclkout1 0 0 0 0 0
acm_mclkout0_sel 0 0 0 0 0
aud_mclkout0 0 0 0 0 0
acm_aud_clk1_sel 0 0 0 0 0
acm_aud_clk1_clk 0 0 0 0 0
acm_aud_clk0_sel 0 0 0 0 0
acm_aud_clk0_clk 0 0 0 0 0
aud_acm_aud_pll_clk0_div 0 0 0 0 0
aud_acm_aud_pll_clk0_clk 0 0 0 0 0
acm_esai1_mclk_sel 0 0 0 0 0
aud_esai1_extal_ipg_clk 0 0 0 0 0
acm_mqs_mclk_sel 0 0 0 0 0
aud_mqs_hm_clk 0 0 0 0 0
acm_spdif1_mclk_sel 0 0 0 0 0
spdif1_tx_clk 0 0 0 0 0
acm_spdif0_mclk_sel 0 0 0 0 0
spdif0_tx_clk 0 0 0 0 0
acm_hdmi_tx_sai0_mclk_sel 0 0 0 0 0
aud_sai_hdmitx0_mclk_clk 0 0 0 0 0
acm_hdmi_rx_sai0_mclk_sel 0 0 0 0 0
aud_sai_hdmirx0_mclk_clk 0 0 0 0 0
acm_sai3_mclk_sel 0 0 0 0 0
aud_sai3_mclk_clk 0 0 0 0 0
acm_sai2_mclk_sel 0 0 0 0 0
aud_sai2_mclk_clk 0 0 0 0 0
acm_sai1_mclk_sel 0 0 0 0 0
aud_sai1_mclk_clk 0 0 0 0 0
acm_sai0_mclk_sel 0 0 0 0 0
aud_sai0_mclk_clk 0 0 0 0 0

0 项奖励
1 回复

554 次查看
jimmychan
NXP TechSupport
NXP TechSupport

which version of bsp are you using?

You can get the latest one from here:

Embedded Linux for i.MX Applications Processors | NXP 

0 项奖励