Dear Team,
Platform: iMX8QM MEK
Software: Android-11 Automotive OS
Number of display : 2 ports LVDS0 & LVDS1
As soon as I switch the board on, NXP logo and progress bar is show like below in the display connected to LVDS-1.
I basically want to disable display driver for LVDS-1 at U-boot stage and on need only to be turned up after Android boot complete. Right now the behaviour is that during U-Boot NXP logo and progress is shown, then display is off and then turned after Android boot compelte.
Please help me disable LVDS-1 @ SPL & U-boot stage. It is very urgent.
Best regards
Libin Jose
Dear Vinod,
I tried your tip. Unfortuantely, the kernel is panic after including this change.
[ 0.621054] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 5.4.47-dirty #5
[ 0.621055] Hardware name: Freescale i.MX8QM MEK (DT)
[ 0.621056] Call trace:
[ 0.621057] dump_backtrace.cfi_jt+0x0/0x4
[ 0.621058] show_stack+0x18/0x24
[ 0.621058] dump_stack+0xb8/0x114
[ 0.621059] panic+0x168/0x3fc
[ 0.621060] nmi_panic+0x98/0xb8
[ 0.621061] arm64_serror_panic+0x74/0x80
[ 0.621061] do_serror+0x15c/0x16c
[ 0.621062] el1_error+0xbc/0x160
[ 0.621063] irq_set_chained_handler_and_data+0x0/0x98
[ 0.621064] platform_drv_probe+0xac/0xf8
[ 0.621065] really_probe+0x30c/0x7ac
[ 0.621065] driver_probe_device+0x64/0x100
[ 0.621066] device_driver_attach+0x6c/0xac
[ 0.621067] __driver_attach+0xdc/0x18c
[ 0.621067] bus_for_each_dev+0xa4/0x118
[ 0.621068] driver_attach+0x24/0x30
[ 0.621069] bus_add_driver+0x100/0x1e0
[ 0.621070] driver_register+0x78/0x114
[ 0.621071] __platform_driver_register+0x44/0x50
[ 0.621071] gpio_mxc_init+0x28/0x34
[ 0.621072] do_one_initcall+0x19c/0x368
[ 0.621073] do_initcall_level+0x198/0x1c4
[ 0.621074] do_basic_setup+0x2c/0x48
[ 0.621075] kernel_init_freeable+0x60/0xdc
[ 0.621075] kernel_init+0x18/0x29c
[ 0.621076] ret_from_fork+0x10/0x18
[ 0.621086] SMP: stopping secondary CPUs
Best regards,
Libin Jose
It is define here,
vendor/nxp/mcu-sdk-auto/SDK_MEK-MIMX8QM/boards/mekmimx8qm/demo_apps/rear_view_camera/cm4_core1/isi_config.h
/*
* For QM RVC, It is required that LVDS1 is used when select LVDS display interface
* DPU1 should be used to accomodate this. Comment it out if use MIPI display interface
*/
#define USE_LVDS1