IMX8MQ constantly restarting (L4.14.98)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8MQ constantly restarting (L4.14.98)

跳至解决方案
1,158 次查看
btodorov
Contributor III

Hello,

I've i.MX8 Quadmax board and I'm trying to run imx-4.14.98-2.0.0_ga on it.

The problem is that the board is constantly restarting at boot:

U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (Mar 10 2022 - 10:17:47 +0000)

CPU: Freescale i.MX8QM revB A53 at 1200 MHz at 28C
Model: Freescale i.MX8QM MEK
Board: iMX8QM MEK
Boot: SD1
DRAM: 5.8 GiB
start sata init
SATA link 0 timeout.
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C0 0x51]
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... Run CMD11 1.8V switch
*** Warning - bad CRC, using default environment

Failed (-5)
[pcie_ctrla_init_rc] LNK DOWN 8600000
In: serial
Out: serial
Err: serial

BuildInfo:
- SCFW f83a2bed, SECO-FW 92ef1143, IMX-MKIMAGE dd023400, ATF 1cb68fa
- U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df

"Synchronous Abort" handler, esr 0x96000004
elr: 0000000080080420 lr : 00000000800439a4 (reloc)
elr: 0000000087ecd420 lr : 0000000087e909a4
x0 : 0000000085678510 x1 : 2e73666b75750ceb
x2 : 0000000000000003 x3 : 000000000000000a
x4 : 0000000000000000 x5 : 000000000000006d
x6 : 0000000085678510 x7 : 0000000000000000
x8 : 0000000085680240 x9 : 0000000000000008
x10: 00000000ffffffd8 x11: 0000000000000006
x12: 000000000001869f x13: 0000000000000200
x14: 000000008565ac1c x15: 00000000ffffffff
x16: 0000000000002080 x17: 0000000000000000
x18: 000000008566ada8 x19: 0000000087efbd60
x20: 0000000000000003 x21: 0000000087efbb50
x22: 0000000085678510 x23: 0000000000000000
x24: 0000000087efcb70 x25: 0000000000000000
x26: 0000000000000000 x27: 0000000000000000
x28: 0000000085678410 x29: 000000008565cb40

Resetting CPU ...

resetting ...

What I did was

$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.0.0_ga.xml
$ MACHINE=imx8qmmek DISTRO=fsl-imx-xwayland source fsl-setup-release.sh -b build-xwayland
$ bitbake fsl-image-validation-imx

Then deployed the images on sd card.

Any idea why is this happening?

 

BR,

Boris

 

0 项奖励
回复
1 解答
1,104 次查看
btodorov
Contributor III

Ok, it looks like I was using corrupted SD card or there were some issues with my card reader. Changed both and now I can boot with my custom build.

Thank you for the support!

在原帖中查看解决方案

0 项奖励
回复
7 回复数
1,150 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励
回复
1,137 次查看
btodorov
Contributor III

After I modified the uuu.auto in L4.14.98 and the demo images are working fine.

Any idea what might be missing in my manual build?

0 项奖励
回复
1,119 次查看
joanxie
NXP TechSupport
NXP TechSupport

the built image should the same as demo images, what built images did  you use? I remembered that I used 4.14.98 built image on my imx8mq board before, don't have such issue

 

标记 (1)
0 项奖励
回复
1,115 次查看
btodorov
Contributor III

I just did"

$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.0.0_ga.xml
$ MACHINE=imx8qmmek DISTRO=fsl-imx-xwayland source fsl-setup-release.sh -b build-xwayland
$ bitbake fsl-image-validation-imx

Then deployed the images on sd card.

Am I missing some step? Something related to uboot?

0 项奖励
回复
1,108 次查看
joanxie
NXP TechSupport
NXP TechSupport

how about replacing demo kernel images by your own built kernel images? could you have the same issue? did you download demo images to the same SD card, everything is ok, right?

0 项奖励
回复
1,105 次查看
btodorov
Contributor III

Ok, it looks like I was using corrupted SD card or there were some issues with my card reader. Changed both and now I can boot with my custom build.

Thank you for the support!

0 项奖励
回复
1,100 次查看
joanxie
NXP TechSupport
NXP TechSupport

good news!

 

0 项奖励
回复