IMX8MQ (chip model: MIMX8MQ6DVAJZAB) dual screen display

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8MQ (chip model: MIMX8MQ6DVAJZAB) dual screen display

201 次查看
ximenbingmeng
Contributor III

1.Does the IMX8MQ chip support dual screen display? What are the restrictions on using it?
2.If the IMX8MQ chip supports dual screen display, what are the resolutions and refresh rates supported by the HDMI interface and MIPI-DSI when used simultaneously?
3. The kernel version we are currently using is 4.14.98. Does this version of the software support dual screen display? How should the device tree be modified if it is supported? Is there a manual available? Are there any tested examples for our reference? Thank you very much
4. If you purchase an official development board, can you directly connect two HDMI interfaces to test dual screen display?
5. Is there a requirement for the size of DDR for dual screen display?
Looking forward to your reply, thank you very much!

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

172 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

A1.yes it can be used, there is not retriction at least

A2. The resolution should be 1080p in both devices

A3. Linux 6.6.3 is the latest one.

A4. Yes, one from mipi_dsi and the other hdmi

A5. None, the same as the Linux BSP  and EVK board has.

 

Regards

0 项奖励
回复