IMX8MQ UART2(SER2) problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8MQ UART2(SER2) problem

940 次查看
prathap_ponnuch
Contributor I

Hi all,

I am trying UART3(SER2 TX and RX) communication.

Following setting are done:

/* ser2 */&uart3 {         pinctrl-names = "default";         pinctrl-0 = <&pinctrl_uart3>;         assigned-clocks = <&clk IMX8MQ_CLK_UART3>;         assigned-clock-parents = <&clk IMX8MQ_CLK_25M>;         uart-has-rtscts;         status = "okay"; };
             /* ser 2 */                pinctrl_uart3: uart3grp {                         fsl,pins = <                                /* SER2_RX */                                MX8MQ_IOMUXC_ECSPI1_SCLK_UART3_DCE_RX           0xe                                /* SER2_TX */                                MX8MQ_IOMUXC_ECSPI1_MOSI_UART3_DCE_TX           0xe                                /* SER2_CTS_N */                                MX8MQ_IOMUXC_ECSPI1_MISO_UART3_DCE_CTS_B        0xe                                /* SER2_RTS_N */                                MX8MQ_IOMUXC_ECSPI1_SS0_UART3_DCE_RTS_B         0xe                        >;                 }; 
After this, in console side we given the following command: note:ttymxc2(tx and rx pin, rts)connected to other host at 115200 baudrate.
root@sm2s-imx8m-qc:~# stty -echo raw speed 115200 < /dev/ttymxc2115200 root@sm2s-imx8m-qc:~# echo "testing" > /dev/ttymxc2              root@sm2s-imx8m-qc:~#    After this commands there is no output in host system?
May i know what is the problem and how to check this uart?
Thanks in advance.

Regards,
prathap

					
				
			
			
				
			
			
				
			
			
			
			
			
			
		
0 项奖励
回复
3 回复数

880 次查看
prathap_ponnuch
Contributor I

Hi Igor,

Thanks for replay.

we are using the following path to modify:

linux-imx/4.14.98-r0/git/arch/arm64/boot/dts/msc$ vi msc-sm2s-imx8m-qc-001.dts

Regards,

prathap

0 项奖励
回复

880 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Prathap

 

if  this is third party software may be suggested to post issue to tech support

of vendor of that software.

 

Best regards
igor

0 项奖励
回复

880 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Prathap

what bsp used in the case, for uart3 dts example one can look at

imx8mq-evk.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

test with uart unit test and Demo Image:

mxc_uart_test\test - imx-test - i.MX Driver Test Application Software 

Demo Image i.MX 8M Quad EVK

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复