Hi,
Customer SKF: is asking for Altium format design files for 8Mplus-EVK Base Board and CPU Module.
As alternative the .ALG files of the two boards which might in case be imported into Altium Tool.
thanks and best regards
Massimo Incerti
解決済! 解決策の投稿を見る。
@Yuri can you pls send the library files of EVK?
Hi Support Team, I am also looking for the ASCII version of these design files. ".alg". Can you please provide them?
Best Regards,
Stuart Mill
Hi,
May I also get the .ALG files of 8MPLUSLPD4-CPU and 8MPLUS-BB ?
Regards and thanks in advance
@zmlopez
Hello,
We do not provide design files for Altium.
Customers can try the following approach:
Regards,
Yuri.
Hello Mr. Yuri
can you please send me the .alg file to me as well..it will be highly appreciated
Dear Yuri,
I´m also looking for tha altium files for the bb46370 and for the pvk46881 boards.
I have the .alg files converted from the .brd original files, but i´m missing the footprints.
Can you help me?
I need to design a custom base board with only a few peripherals with strong space constraints (thinking on 100K boards and the lack of the complete altium project is delaying the project.
Thanks in advance.
marcos.-
Hi, Yuri.
Can you please send a reference on where we can load schematic/reference files - we are planning to start working on SOM based on i.MX8M.
The board we have and ideally for which we need design files is 8MPLUSPLD4-EVK
Thanks in advance.
Sergei Danielian
@sergeidanielian
Hello,
Please use the following resources:
https://www.nxp.com/webapp/Download?colCode=8MPLUSLPD4-PWR-DESIGN-FILES
https://www.nxp.com/downloads/en/schematics/8MPLUS-BB.zip
https://www.nxp.com/downloads/en/schematics/8MPLUSLPD4-CPU.zip
Regards,
Yuri.
Hi Yuri,
I am designing a new platform based on imx8mp, it would be useful for me to have the .alg files (or Altium files) of the CPU and BaseBorad EVK.
Thanks in advance.
Diego.
Thanks Yuri.