IMX8MP Custom Board firmware-nxp-wifi is not being built

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MP Custom Board firmware-nxp-wifi is not being built

Jump to solution
599 Views
Wobaffet
Senior Contributor I

I am trying to port 88w8987 based wifi/bt modem with sdio interface.

I've added IMAGE_INSTALL += " firmware-nxp-wifi"  

But for the generated image with yocto project, which I use the latest BSP. I don't see any kernel objects should be built with this recipe such as moal.ko.

root@imx8mp-lpddr4-evk:/# ls lib/firmware/
jailhouse.bin        tee-header_v2.bin    tee-pageable_v2.bin  tee-pager_v2.bin     tee-raw.bin          tee.bin              tee.elf         

I don't even have a nxp directory on the firmware folder.

What could be the reason?

Thank you in advance!

Best Regards.

0 Kudos
Reply
1 Solution
549 Views
cdoumenc
NXP Employee
NXP Employee

You have to push the 2 drivers .ko and the fw .bin from the building machine to the target.

You will find these files here :
wlan_src/*.ko (ex : mlan.ko et moal.ko)
FwImage/*.bin (ex : sduart8987_combo_v0.bin)

fw .bin has to be put in target directory  /lib/firmware/nxp/

Then kernel modules have to be loaded as explained in doc UM11483 (chap "5 Bring-up of Wi-Fi") you will find on product page https://www.nxp.com/products/wireless-connectivity/wi-fi-plus-bluetooth-plus-802-15-4/2-4-5-ghz-dual...

Here is the direct link : https://www.nxp.com/webapp/Download?colCode=UM11483

 

View solution in original post

5 Replies
564 Views
cdoumenc
NXP Employee
NXP Employee

Could you have a look at NXP doc UM11675 (especially chapter "6.1 i.MX 8M evaluation platform with Yocto"), please ?

0 Kudos
Reply
561 Views
Wobaffet
Senior Contributor I

Yes, that's the manual I've followed when cross-compiling the firmware, my problem is how I can import these generated binaries and kernel objects from the cross-compilation with the image I've been building with Yocto image.

Thanks!

0 Kudos
Reply
550 Views
cdoumenc
NXP Employee
NXP Employee

You have to push the 2 drivers .ko and the fw .bin from the building machine to the target.

You will find these files here :
wlan_src/*.ko (ex : mlan.ko et moal.ko)
FwImage/*.bin (ex : sduart8987_combo_v0.bin)

fw .bin has to be put in target directory  /lib/firmware/nxp/

Then kernel modules have to be loaded as explained in doc UM11483 (chap "5 Bring-up of Wi-Fi") you will find on product page https://www.nxp.com/products/wireless-connectivity/wi-fi-plus-bluetooth-plus-802-15-4/2-4-5-ghz-dual...

Here is the direct link : https://www.nxp.com/webapp/Download?colCode=UM11483

 

588 Views
cdoumenc
NXP Employee
NXP Employee
0 Kudos
Reply
584 Views
Wobaffet
Senior Contributor I

Hello, I’ve cross compiled the driver but to deploy the binaries to the board with the custom image on yocto environment I need a recipe.

0 Kudos
Reply