Hi,
We are able to hear output through HDMI, but if the media volume is adjusted below 50%, the sound becomes barely audible.
Settings -> Sound & Vibration -> Media Volume
Audio HDMI is registered under
[ 13.899336] input: audio-hdmi HDMI Jack as /devices/platform/sound-hdmi/sound/card2/input2
We tried tinymix we didnt get any results.
evk_8mp:/ # tinymix -D 2
Mixer name: 'audio-hdmi'
Number of controls: 5
ctl type num name value
0 BOOL 1 HDMI Jack On
1 INT 8 Playback Channel Map 0 0 0 0 0 0 0 0
2 IEC958 1 IEC958 Playback Mask unknown
3 IEC958 1 IEC958 Playback Default unknown
4 BYTE 128 ELD 10 00 08 00 6b 10 .. .. .. .. .. ..
Is there any suggestion to increase the HDMI-audio threshold so that audible sound when below 50%.
Hi
It looks like you need add audo gain config file in your aosp image, not prebuilt image.
Best Regards
Zhiming