IMX8MN UART1 can not receive data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MN UART1 can not receive data

Jump to solution
1,276 Views
link
Contributor III

Hi all:

        Now we use UART1 of IMX8MN to communicate with PC. The device can send data, but cannot receive data. The correct waveform can be measured at the RX end of the device. It is OK to send and receive data in the same program on UART2.

      To confirm the question, use imx8mnevk as a comparison. we run unit_tests to text /dev/ttymxc0.
Snipaste_2021-11-02_19-38-41.bmp
For mxc_uart_test.out:
write and read data are OK

---- Running < ./mxc_uart_test.out > test ----

/dev/ttymxc0 opened
Attributes set
Test: IOCTL Set
Data Written= Test
Data Read back= Test

----  Test < /dev/ttymxc0 > ended  ----



For mxc_uart_stress_test.out
write data is OK, but tne receive data is empty.

clipboard.png

What may the cause? Does UART1 need additional software configuration for serial port

Thanks!

Labels (1)
0 Kudos
Reply
1 Solution
1,256 Views
link
Contributor III

 

			uart1: serial@30860000 {
				compatible = "fsl,imx8mn-uart", "fsl,imx6q-uart";
				reg = <0x30860000 0x10000>;
				interrupts = <GIC_SPI 26 IRQ_TYPE_LEVEL_HIGH>;
				clocks = <&clk IMX8MN_CLK_UART1_ROOT>,
					 <&clk IMX8MN_CLK_UART1_ROOT>;
				clock-names = "ipg", "per";
				dmas = <&sdma1 22 4 0>, <&sdma1 23 4 0>;
				dma-names = "rx", "tx";
				status = "disabled";
			};

 

 

sdma.bin is not integrated in rootFS.UART1 depends on SDMA. So the UART1 function is abnormal

 

View solution in original post

0 Kudos
Reply
2 Replies
1,257 Views
link
Contributor III

 

			uart1: serial@30860000 {
				compatible = "fsl,imx8mn-uart", "fsl,imx6q-uart";
				reg = <0x30860000 0x10000>;
				interrupts = <GIC_SPI 26 IRQ_TYPE_LEVEL_HIGH>;
				clocks = <&clk IMX8MN_CLK_UART1_ROOT>,
					 <&clk IMX8MN_CLK_UART1_ROOT>;
				clock-names = "ipg", "per";
				dmas = <&sdma1 22 4 0>, <&sdma1 23 4 0>;
				dma-names = "rx", "tx";
				status = "disabled";
			};

 

 

sdma.bin is not integrated in rootFS.UART1 depends on SDMA. So the UART1 function is abnormal

 

0 Kudos
Reply
1,266 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yanlin

 

may be recommended to check if signal present on uart1 pad with oscilloscope,

for software check if IOMUXC_UART1_RX_SELECT_INPUT configured properly, it is described in

sect.8.2.5.261 Select Input Register (IOMUXC_UART1_RX_SELECT_INPUT)

i.MX 8M Nano Applications Processor Reference Manual

 

Best regards
igor

0 Kudos
Reply