IMX8MM in Yocto 5.15.52 rust-llvm_1.59.0.bb do_compile failed.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8MM in Yocto 5.15.52 rust-llvm_1.59.0.bb do_compile failed.

跳至解决方案
3,290 次查看
charleshuang
Senior Contributor II

Hi NXP Team

 

ERROR: Task (virtual:native:/home/adv/adv-release-bsp/sources/poky/meta/recipes-devtools/rust/rust-llvm_1.59.0.bb:do_compile) failed with exit code '1'

In file included from /home/adv/adv-release-bsp/build_5721/tmp/work/x86_64-linux/rust-llvm-native/1.59.0-r0/rustc-1.59.0-src/src/llvm-project/llvm/lib/Target/AArch64/AArch64ISelDAGToDAG.cpp:323:

/home/adv/adv-release-bsp/build_5721/tmp/work/x86_64-linux/rust-llvm-native/1.59.0-r0/build/lib/Target/AArch64/AArch64GenDAGISel.inc: In member function ‘void {anonymous}::AArch64DAGToDAGISel::SelectCode(llvm::SDNode*)’:

/home/adv/adv-release-bsp/build_5721/tmp/work/x86_64-linux/rust-llvm-native/1.59.0-r0/build/lib/Target/AArch64/AArch64GenDAGISel.inc:121066:5: error: ‘OPC_RecordChilD2’ was not declared in this scope; did you mean ‘OPC_RecordChild2’?

charleshuang_0-1670913113948.png

Do you have any idea about to fixed the issue?  Thanks

0 项奖励
1 解答
3,263 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @charleshuang 

I hope you are doing well.

It seems you are using old version of rust-llvm. Please try with the latest version of rust-llvm.

Thanks & Regards

Sanket Parekh

在原帖中查看解决方案

0 项奖励
12 回复数
434 次查看
lkraak
Contributor I

Hey, bump

0 项奖励
421 次查看
charleshuang
Senior Contributor II

Hi NXP Team 

Sorry for late reply. We already find the solution.

0 项奖励
435 次查看
lkraak
Contributor I

bump

0 项奖励
1,165 次查看
yonguklee
Contributor I

i've got the same problem above

please, let me know how to update rust-llvm ??

0 项奖励
3,129 次查看
Ferromagnetic
Contributor II

I have the same problem with standard build for imx8qxpc0mek, is will be fixed on official repo?

0 项奖励
3,264 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @charleshuang 

I hope you are doing well.

It seems you are using old version of rust-llvm. Please try with the latest version of rust-llvm.

Thanks & Regards

Sanket Parekh

0 项奖励
3,251 次查看
charleshuang
Senior Contributor II
Hi Sanket_Parekh
How to do about update latest version of rust-llvm.
Please provide the solution, Thanks.
0 项奖励
3,228 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @charleshuang 

One can take the latest source of rust llvm from link. One can follow link to integrate new source in existing yocto repository.

Thanks & Regards

Sanket Parekh

0 项奖励
2,979 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @charleshuang 

Any updates from your side?

Thanks & Regards

Sanket Parekh

0 项奖励
3,205 次查看
Marco_Zaccheria
NXP Employee
NXP Employee

Hi @Sanket_Parekh,

sorry to jump in, looks like the customer is not doing any BSP customization, instead this issue appears by just following our standard instructions for the build. This means we have a problem on our distribution, and so we definitely have to fix it.

I actually see other similar issues filed, and I have yet another customer who encountered this issue by just building our standard BSP for the i.MX8MNano EVK. This means we shoud definitily file a bug to our SE team, if you don't mind I can do that, and point you to that case so that you can follow the progress.

Meanwhile, could you please provide here more detailed instructions on how to replace the failing package with a more up-to-date one that doesn't show this issue?

Thank you

   Marco

0 项奖励
1,303 次查看
snoophogg
Contributor I

It would be great if someone could provide instructions on how to replace the package with the newer version.  Thanks

0 项奖励
2,998 次查看
Lisbravo
Contributor I

bump