IMX8MM PMIC_ON_REQ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MM PMIC_ON_REQ

1,565件の閲覧回数
santhosh2
Contributor IV

Is there any way to toggle the  PMIC_ON_REQ using software in IMX8MM

 

Regards

Santhosh

0 件の賞賛
返信
7 返答(返信)

1,554件の閲覧回数
Yuri
NXP Employee
NXP Employee

@santhosh2 
Hello,

  
  The PMIC_ON_REQ signal can be controlled by the LPCR[TOP] and
LPCR[DP_EN] bits, say, when the 'poweroff' command is issued in Linux.

   For power on only ONOFF pin can be used.

Regards,
Yuri.

0 件の賞賛
返信

1,549件の閲覧回数
santhosh2
Contributor IV

Hello Yuri,

I have tried this method, But the PMIC_ON_REQ pin toggles only when the switch is pressed as mentioned in the data sheet.

PMIC_ON_REQ.png

Since I want to Control this PMIC_ON_REQ via software to reset the entire PMIC without using the switch, Is there any other way?

Regards

Santhosh

タグ(1)
0 件の賞賛
返信

1,539件の閲覧回数
Yuri
NXP Employee
NXP Employee

@santhosh2 

  Also, LPCR[DP_EN]  should be set.

 

~Yuri.

0 件の賞賛
返信

1,530件の閲覧回数
santhosh2
Contributor IV

hello yuri,

I tried it is not working for me, Any other things needs to be done

Regards

santhosh

0 件の賞賛
返信

1,516件の閲覧回数
Yuri
NXP Employee
NXP Employee

@santhosh2 
Hello,

   is Linux command "poweroff" working on Your board?

Regards,
Yuri.

0 件の賞賛
返信

1,503件の閲覧回数
santhosh2
Contributor IV

Power off command is available, but when poweroff command fired, the system power's off but reboot doesn't happen, Please advice any next step to try?

 

poweroff1.pngpoweroff2.png

タグ(1)
0 件の賞賛
返信

1,494件の閲覧回数
Yuri
NXP Employee
NXP Employee

@santhosh2 
Hello,

   let me know how LPCR[TOP] , LPCR[DP_EN] are written in Your tests.

Regards,
Yuri.

0 件の賞賛
返信