IMX8MM ANDROID13 BUILD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8MM ANDROID13 BUILD

1,338 次查看
gravity_one
Contributor III

Hello Guys,

PLATFORM_VERSION=13
TARGET_PRODUCT=evk_8mm
TARGET_BUILD_VARIANT=userdebug
TARGET_BUILD_TYPE=release
TARGET_ARCH=arm64
TARGET_ARCH_VARIANT=armv8-a
TARGET_CPU_VARIANT=cortex-a53
TARGET_2ND_ARCH=arm
TARGET_2ND_ARCH_VARIANT=armv7-a-neon
TARGET_2ND_CPU_VARIANT=cortex-a9
HOST_ARCH=x86_64
HOST_2ND_ARCH=x86
HOST_OS=linux
HOST_OS_EXTRA=Linux-5.15.0-56-generic-x86_64-Ubuntu-18.04.6-LTS
HOST_CROSS_OS=windows
HOST_CROSS_ARCH=x86
HOST_CROSS_2ND_ARCH=x86_64
HOST_BUILD_TYPE=release
BUILD_ID=TP1A.221005.002
OUT_DIR=out
PRODUCT_SOONG_NAMESPACES=device/generic/goldfish device/generic/goldfish-opengl external/mesa3d vendor/nxp-opensource/imx/power hardware/google/pixel hardware/google/camera vendor/nxp-opensource/imx/camera vendor/partner_gms
============================================



[ 98% 417/422] analyzing Android.bp files and generating ninja file at out/soong/build.ninja
FAILED: out/soong/build.ninja
cd "$(dirname "out/host/linux-x86/bin/soong_build")" && BUILDER="$PWD/$(basename "out/host/linux-x86/bin/soong_build")" && cd / && env -i  "$BUILDER"     --top "$TOP"     --soong_out "out/soong"     --out "out"     -o out/soong/build.ninja --globListDir build --globFile out/soong/globs-build.ninja -t -l out/.module_paths/Android.bp.list --available_env out/soong/soong.environment.available --used_env out/soong/soong.environment.used.build Android.bp
error: vendor/nxp/vpu_wrapper/Android.bp:85:1: "lib_vpu_wrapper" depends on undefined module "libcodec"
error: vendor/nxp/vpu_wrapper/Android.bp:85:1: "lib_vpu_wrapper" depends on undefined module "libhantro"
error: vendor/nxp/vpu_wrapper/Android.bp:85:1: "lib_vpu_wrapper" depends on undefined module "libcodec_enc"
error: vendor/nxp/vpu_wrapper/Android.bp:85:1: "lib_vpu_wrapper" depends on undefined module "libhantro_h1"
02:06:23 soong bootstrap failed with: exit status 1

#### failed to build some targets (01:52 (mm:ss)) ####

build@9dc8c7c99f08:~/androidserver/android_build$
build@9dc8c7c99f08:~/androidserver/android_build$
build@9dc8c7c99f08:~/androidserver/android_build$
build@9dc8c7c99f08:~/androidserver/android_build$
0 项奖励
4 回复数

169 次查看
giampietroghizz
Contributor II

hi,
I am trying to do the same thing.
I am following the directions given in this document:
https://www.nxp.com/docs/en/user-guide/Android_Auto_User's_Guide.pdf

however i see that the “build” folder is not created with the envsetup.sh file

could you give me some pointers?

thanks

0 项奖励

1,311 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @gravity_one 

Do you still have the problem? 

Would suggest you check the necessary packages installed on your host? both of android and additional packages from NXP as stated in Android user guide.

and have you run command source for i.MX Android proprietary source code package

You might need to try to make clean and then rebuild.

 

Best regards

Harvey

0 项奖励

1,008 次查看
Danilo3
Contributor III

Hello,

I have a very similar issue when building imx-automotive-13.0.0_1.1.0, mek_8q_car2-userdebug.

I followed all the steps indicated in the Android User's Guide (Sectio 3 - Building the Android platform for i.MX). I successfully fetched the whole source for the build.

This is the "lunch mek_8q_car2-userdebug" output:

===========================================
PLATFORM_VERSION_CODENAME=REL
PLATFORM_VERSION=13
TARGET_PRODUCT=mek_8q_car2
TARGET_BUILD_VARIANT=userdebug
TARGET_BUILD_TYPE=release
TARGET_ARCH=arm64
TARGET_ARCH_VARIANT=armv8-a
TARGET_CPU_VARIANT=cortex-a53
TARGET_2ND_ARCH=arm
TARGET_2ND_ARCH_VARIANT=armv7-a-neon
TARGET_2ND_CPU_VARIANT=cortex-a9
HOST_ARCH=x86_64
HOST_2ND_ARCH=x86
HOST_OS=linux
HOST_OS_EXTRA=Linux-5.15.0-76-generic-x86_64-Ubuntu-20.04.6-LTS
HOST_CROSS_OS=windows
HOST_CROSS_ARCH=x86
HOST_CROSS_2ND_ARCH=x86_64
HOST_BUILD_TYPE=release
BUILD_ID=TP1A.221005.002
OUT_DIR=out
PRODUCT_SOONG_NAMESPACES=device/generic/goldfish device/generic/goldfish-opengl external/mesa3d vendor/nxp-opensource/imx/power hardware/google/pixel hardware/google/camera vendor/nxp-opensource/imx/camera vendor/partner_gas
============================================

and these are the errors I get when running ./imx-make.sh :

FAILED: out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/CarDialerApp.jar
rm -rf "out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/classes" "out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/anno" "out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/srcjars" "out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/CarDialerApp.jar" && mkdir -p "out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/classes" "out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/anno" "out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/srcjars" && out/host/linux-x86/bin/zipsync -d out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/srcjars -l out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/srcjars/list -f "*.java" out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/gen/android/R.srcjar && (if [ -s out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/srcjars/list ] || [ -s out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/CarDialerApp.jar.rsp ] ; then out/host/linux-x86/bin/soong_javac_wrapper prebuilts/jdk/jdk11/linux-x86/bin/javac -J-Xmx2048M -J-XX:OnError="cat hs_err_pid%p.log" -J-XX:CICompilerCount=6 -J-XX:+UseDynamicNumberOfGCThreads -J-XX:+TieredCompilation -J-XX:TieredStopAtLevel=1 -Xmaxerrs 9999999 -encoding UTF-8 -sourcepath "" -g -XDskipDuplicateBridges=true -XDstringConcat=inline -processorpath out/soong/.intermediates/external/dagger2/dagger2-compiler/linux_glibc_common/withres/dagger2-compiler.jar:out/soong/.intermediates/external/dagger2/hilt_android_entry_point_processor/linux_glibc_common/combined/hilt_android_entry_point_processor.jar:out/soong/.intermediates/external/dagger2/hilt_aggregated_deps_processor/linux_glibc_common/combined/hilt_aggregated_deps_processor.jar:out/soong/.intermediates/external/dagger2/hilt_alias_of_processor/linux_glibc_common/combined/hilt_alias_of_processor.jar:out/soong/.intermediates/external/dagger2/hilt_define_component_processor/linux_glibc_common/combined/hilt_define_component_processor.jar:out/soong/.intermediates/external/dagger2/hilt_generates_root_input_processor/linux_glibc_common/withres/hilt_generates_root_input_processor.jar:out/soong/.intermediates/external/dagger2/hilt_originating_element_processor/linux_glibc_common/combined/hilt_originating_element_processor.jar:out/soong/.intermediates/external/dagger2/hilt_root_processor/linux_glibc_common/combined/hilt_root_processor.jar:out/soong/.intermediates/external/dagger2/hilt_viewmodel_processor/linux_glibc_common/combined/hilt_viewmodel_processor.jar:out/soong/.intermediates/prebuilts/sdk/current/androidx/androidx.room_room-compiler-plugin/linux_glibc_common/combined/androidx.room_room-compiler-plugin.jar -processor dagger.internal.codegen.ComponentProcessor,dagger.hilt.android.processor.internal.androidentrypoint.AndroidEntryPointProcessor,dagger.hilt.processor.internal.aggregateddeps.AggregatedDepsProcessor,dagger.hilt.processor.internal.aliasof.AliasOfProcessor,dagger.hilt.processor.internal.definecomponent.DefineComponentProcessor,dagger.hilt.processor.internal.generatesrootinput.GeneratesRootInputProcessor,dagger.hilt.processor.internal.originatingelement.OriginatingElementProcessor,dagger.hilt.processor.internal.root.RootProcessor,dagger.hilt.android.processor.internal.viewmodel.ViewModelProcessor,androidx.room.RoomProcessor -Xlint:-dep-ann --system=out/soong/.intermediates/build/soong/java/core-libraries/core-public-stubs-system-modules/android_common/system -classpath out/soong/.intermediates/frameworks/base/android_system_stubs_current/android_common/turbine-combined/android_system_stubs_current.jar:out/soong/.intermediates/packages/services/Car/car-lib/android.car-system-stubs/android_common/turbine-combined/android.car-system-stubs.jar:out/soong/.intermediates/packages/apps/Car/libs/car-apps-common/car-apps-common-prebuilt/android_common/aar/classes-combined.jar:out/soong/.intermediates/packages/apps/Car/libs/car-assist-lib/car-assist-lib-prebuilt/android_common/aar/classes-combined.jar:out/soong/.intermediates/packages/apps/Car/libs/car-telephony-common/car-telephony-common-prebuilt/android_common/aar/classes-combined.jar:out/soong/.intermediates/packages/apps/Car/libs/car-messenger-common/car-messenger-common/android_common/turbine-combined/car-messenger-common.jar:out/soong/.intermediates/packages/apps/Car/libs/car-ui-lib/car-ui-lib-prebuilt/android_common/aar/classes-combined.jar:out/soong/.intermediates/packages/apps/Car/libs/car-uxr-client-lib/car-uxr-client-lib-prebuilt/android_common/aar/classes-combined.jar:out/soong/.intermediates/external/error_prone/error_prone_annotations/android_common/combined/error_prone_annotations.jar:out/soong/.intermediates/external/guava/guava/android_common/turbine-combined/guava.jar:out/soong/.intermediates/prebuilts/maven_repo/bumptech/glide-prebuilt/android_common/aar/classes-combined.jar:out/soong/.intermediates/prebuilts/maven_repo/bumptech/glide-gifdecoder-prebuilt/android_common/aar/classes-combined.jar:out/soong/.intermediates/prebuilts/maven_repo/bumptech/glide-disklrucache-prebuilt/android_common/aar/classes-combined.jar:out/soong/.intermediates/prebuilts/maven_repo/bumptech/glide-annotation-and-compiler-prebuilt/android_common/jetifier/glide-annotation-and-compiler-prebuilt.jar:out/soong/.intermediates/external/dagger2/hilt_android/android_common/combined/hilt_android.jar:out/soong/.intermediates/prebuilts/sdk/current/extras/constraint-layout-x/androidx-constraintlayout_constraintlayout/android_common/turbine-combined/androidx-constraintlayout_constraintlayout.jar:out/soong/.intermediates/prebuilts/sdk/current/extras/constraint-layout-x/androidx-constraintlayout_constraintlayout-solver/android_common/turbine-combined/androidx-constraintlayout_constraintlayout-solver.jar:out/soong/.intermediates/prebuilts/sdk/current/androidx/androidx.cardview_cardview/android_common/turbine-combined/androidx.cardview_cardview.jar:out/soong/.intermediates/prebuilts/sdk/current/androidx-legacy/androidx.legacy_legacy-support-v4/android_common/turbine-combined/androidx.legacy_legacy-support-v4.jar:out/soong/.intermediates/prebuilts/sdk/current/androidx/androidx.lifecycle_lifecycle-common-java8/android_common/turbine-combined/androidx.lifecycle_lifecycle-common-java8.jar:out/soong/.intermediates/prebuilts/sdk/current/androidx-legacy/androidx.lifecycle_lifecycle-extensions/android_common/turbine-combined/androidx.lifecycle_lifecycle-extensions.jar:out/soong/.intermediates/prebuilts/sdk/current/androidx/androidx.preference_preference/android_common/turbine-combined/androidx.preference_preference.jar:out/soong/.intermediates/prebuilts/sdk/current/androidx/androidx.recyclerview_recyclerview/android_common/turbine-combined/androidx.recyclerview_recyclerview.jar:out/soong/.intermediates/prebuilts/sdk/current/androidx/androidx.room_room-runtime/android_common/turbine-combined/androidx.room_room-runtime.jar:out/soong/.intermediates/prebuilts/sdk/current/androidx/androidx.sqlite_sqlite/android_common/turbine-combined/androidx.sqlite_sqlite.jar:out/soong/.intermediates/prebuilts/sdk/current/androidx/androidx.sqlite_sqlite-framework/android_common/turbine-combined/androidx.sqlite_sqlite-framework.jar:out/soong/.intermediates/prebuilts/sdk/current/androidx/androidx.exifinterface_exifinterface/android_common/turbine-combined/androidx.exifinterface_exifinterface.jar:out/soong/.intermediates/packages/apps/Car/Dialer/framework/car-dialer-framework-dep/android_common/combined/car-dialer-framework-dep.jar -source 11 -target 11 -d out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/classes -s out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/anno @out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/CarDialerApp.jar.rsp @out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/srcjars/list ; fi ) && out/host/linux-x86/bin/soong_zip -jar -o out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/CarDialerApp.jar -C out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/classes -D out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/classes && rm -rf "out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/srcjars"
packages/apps/Car/Dialer/src/com/android/car/dialer/inject/DialerModules.java:36: error: package com.android.car.telephony.calling does not exist
import com.android.car.telephony.calling.InCallServiceManager;
^
packages/apps/Car/Dialer/src/com/android/car/dialer/inject/DialerModules.java:112: error: cannot find symbol
static InCallServiceManager provideInCallServiceManager() {
^
symbol: class InCallServiceManager
location: class AppModule
packages/apps/Car/Dialer/src/com/android/car/dialer/inject/DialerModules.java:117: error: cannot find symbol
static List<Call> provideCallList(InCallServiceManager inCallServiceManager) {
^
symbol: class InCallServiceManager
location: class AppModule
packages/apps/Car/Dialer/src/com/android/car/dialer/telecom/InCallServiceImpl.java:33: error: package com.android.car.telephony.calling does not exist
import com.android.car.telephony.calling.InCallServiceManager;
^
packages/apps/Car/Dialer/src/com/android/car/dialer/telecom/InCallServiceImpl.java:61: error: cannot find symbol
@Inject InCallServiceManager mInCallServiceManager;
^
symbol: class InCallServiceManager
location: class InCallServiceImpl
packages/apps/Car/Dialer/src/com/android/car/dialer/telecom/ProjectionCallHandler.java:35: error: package com.android.car.telephony.calling does not exist
import com.android.car.telephony.calling.InCallServiceManager;
^
packages/apps/Car/Dialer/src/com/android/car/dialer/telecom/LocalCallHandler.java:29: error: package com.android.car.telephony.calling does not exist
import com.android.car.telephony.calling.InCallServiceManager;
^
packages/apps/Car/Dialer/src/com/android/car/dialer/telecom/LocalCallHandler.java:54: error: cannot find symbol
private final InCallServiceManager mInCallServiceManager;
^
symbol: class InCallServiceManager
location: class LocalCallHandler
packages/apps/Car/Dialer/src/com/android/car/dialer/telecom/LocalCallHandler.java:88: error: cannot find symbol
InCallServiceManager inCallServiceManager,
^
symbol: class InCallServiceManager
location: class LocalCallHandler
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/InCallViewModel.java:31: error: package com.android.car.telephony.calling does not exist
import com.android.car.telephony.calling.AudioRouteLiveData;
^
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/InCallViewModel.java:32: error: package com.android.car.telephony.calling does not exist
import com.android.car.telephony.calling.CallDetailLiveData;
^
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/InCallViewModel.java:33: error: package com.android.car.telephony.calling does not exist
import com.android.car.telephony.calling.CallStateLiveData;
^
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/InCallViewModel.java:35: error: package com.android.car.telephony.calling does not exist
import com.android.car.telephony.calling.SupportedAudioRoutesLiveData;
^
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/InCallViewModel.java:62: error: package AudioRouteLiveData does not exist
private final AudioRouteLiveData.Factory mAudioRouteLiveDataFactory;
^
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/InCallViewModel.java:63: error: package SupportedAudioRoutesLiveData does not exist
private final SupportedAudioRoutesLiveData.Factory mSupportedAudioRoutesLiveDataFactory;
^
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/InCallViewModel.java:76: error: cannot find symbol
private final CallDetailLiveData mCallDetailLiveData;
^
symbol: class CallDetailLiveData
location: class InCallViewModel
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/InCallViewModel.java:82: error: cannot find symbol
private final CallDetailLiveData mSecondaryCallDetailLiveData;
^
symbol: class CallDetailLiveData
location: class InCallViewModel
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/InCallViewModel.java:90: error: cannot find symbol
private final AudioRouteLiveData mAudioRouteLiveData;
^
symbol: class AudioRouteLiveData
location: class InCallViewModel
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/InCallViewModel.java:91: error: cannot find symbol
private final SupportedAudioRoutesLiveData mSupportedAudioRoutesLiveData;
^
symbol: class SupportedAudioRoutesLiveData
location: class InCallViewModel
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/InCallViewModel.java:117: error: package AudioRouteLiveData does not exist
AudioRouteLiveData.Factory audioRouteLiveDataFactory,
^
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/InCallViewModel.java:118: error: package SupportedAudioRoutesLiveData does not exist
SupportedAudioRoutesLiveData.Factory supportedAudioRouteLiveDataFactory,
^
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/OnGoingCallControllerBarFragment.java:48: error: package com.android.car.telephony.calling does not exist
import com.android.car.telephony.calling.InCallServiceManager;
^
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/OnGoingCallControllerBarFragment.java:90: error: cannot find symbol
@Inject InCallServiceManager mInCallServiceManager;
^
symbol: class InCallServiceManager
location: class OnGoingCallControllerBarFragment
packages/apps/Car/Dialer/src/com/android/car/dialer/telecom/InCallServiceImpl.java:49: error: [ComponentProcessor:MiscError] dagger.internal.codegen.ComponentProcessor was unable to process this class because not all of its dependencies could be resolved. Check for compilation errors or a circular dependency with generated code.
public class InCallServiceImpl extends Hilt_InCallServiceImpl {
^
packages/apps/Car/Dialer/src/com/android/car/dialer/telecom/LocalCallHandler.java:50: error: [ComponentProcessor:MiscError] dagger.internal.codegen.ComponentProcessor was unable to process this class because not all of its dependencies could be resolved. Check for compilation errors or a circular dependency with generated code.
public class LocalCallHandler
^
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/InCallViewModel.java:58: error: [ComponentProcessor:MiscError] dagger.internal.codegen.ComponentProcessor was unable to process this class because not all of its dependencies could be resolved. Check for compilation errors or a circular dependency with generated code.
public class InCallViewModel extends ViewModel {
^
packages/apps/Car/Dialer/src/com/android/car/dialer/ui/activecall/OnGoingCallControllerBarFragment.java:67: error: [ComponentProcessor:MiscError] dagger.internal.codegen.ComponentProcessor was unable to process this class because not all of its dependencies could be resolved. Check for compilation errors or a circular dependency with generated code.
public class OnGoingCallControllerBarFragment extends Hilt_OnGoingCallControllerBarFragment {
^
packages/apps/Car/Dialer/src/com/android/car/dialer/inject/DialerModules.java:67: error: [ComponentProcessor:MiscError] dagger.internal.codegen.ComponentProcessor was unable to process this class because not all of its dependencies could be resolved. Check for compilation errors or a circular dependency with generated code.
public static final class AppModule {
^
out/soong/.intermediates/packages/apps/Car/Dialer/CarDialerApp/android_common/javac/anno/com/android/car/dialer/DialerApplication_HiltComponents.java:178: error: [ComponentProcessor:MiscError] dagger.internal.codegen.ComponentProcessor was unable to process this class because not all of its dependencies could be resolved. Check for compilation errors or a circular dependency with generated code.
public abstract static class SingletonC implements DialerApplication_GeneratedInjector,
^
29 errors
[ 14% 294/1971] //packages/modules/Connectivity/Tethering:TetheringNext javac [common apex30]
[ 14% 295/1971] //art/build/apex:com.android.art sign compressedApex [common]
[ 15% 296/1971] //packages/modules/Connectivity/Tethering:TetheringApiCurrentLib javac [common apex30]
warning: Supported source version 'RELEASE_9' from annotation processor 'android.processor.compat.unsupportedappusage.UnsupportedAppUsageProcessor' less than -source '11'
1 warning
[ 15% 297/1971] //system/security/keystore2/aidl:android.security.remoteprovisioning-rust rustc android_security_remoteprovisioning.rs
[ 15% 298/1971] //packages/apps/Gallery2:Gallery2 jarjar [common]
[ 15% 299/1971] //external/setupdesign:setupdesign javac [common]
[ 15% 300/1971] //packages/apps/ImsServiceEntitlement:ImsServiceEntitlementLib turbine [common]
[ 15% 301/1971] build out/target/product/mek_8q/obj/PACKAGING/vendor_boot-debug_intermediates/vendor_ramdisk-debug.cpio.lz4
[ 15% 302/1971] build out/target/product/mek_8q/obj/PACKAGING/vendor_boot-test-harness_intermediates/vendor_ramdisk-test-harness.cpio.lz4
[ 15% 303/1971] //external/perfetto:perfetto_trace_java_protos javac [common]
[ 15% 304/1971] //system/extras/profcollectd/libprofcollectd:libprofcollectd rustc lib.rs
[ 15% 305/1971] //external/setupdesign/lottie_loading_layout:setupdesign-lottie-loading-layout turbine [common]
[ 15% 306/1971] //system/hardware/interfaces/keystore2/aidl:android.system.keystore2-V2-rust rustc android_system_keystore2_V2.rs
[ 15% 307/1971] //packages/modules/Bluetooth/system:libbt_facade_proto rustc mod_facade.rs [apex33]
[ 15% 308/1971] //packages/apps/ImsServiceEntitlement:ImsServiceEntitlementLib javac [common]
[ 15% 309/1971] //frameworks/base/packages/SettingsLib:SettingsLib kotlinc [common]
[ 15% 310/1971] //frameworks/base:framework-minus-apex jarjar [common]
[ 15% 311/1971] //external/uwb/src:libuwb_uci_rust rustc rust/lib.rs [apex33]
[ 15% 312/1971] //frameworks/base/services:services-non-updatable-stubs metalava merged [common]
ninja: build stopped: subcommand failed.
10:41:34 ninja failed with: exit status 1

#### failed to build some targets (36 seconds) ####

It seems many packages are missing.

Thank you

0 项奖励

945 次查看
Danilo3
Contributor III

Hello,

I'm now using release AAOS 13.0.0_1.3.0 which can be built without any issues.

0 项奖励