IMX8M's USB Port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M's USB Port

681件の閲覧回数
xuyuanzhi
Contributor I

When download the Imx8m's Image, the Imx8m EVK board use the J901 USB TYPE-C conncector. I wonder when use the Mfgtool download the Image through this port , the usb is running USB2.0 or USB3.0?  When downloading Image, if only the usb1_dp and usb1_dn is needed, the other usb signals is not neceasary? Thank you!

ラベル(1)
0 件の賞賛
1 返信

424件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi xu,

When using i.MX8 EVK and the mfgtool use USB3.0.

Regards

0 件の賞賛