IMX8M-Plus vs IMX8-DualXPlus power usage and heat

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M-Plus vs IMX8-DualXPlus power usage and heat

Jump to solution
1,371 Views
TerryBarnaby1
Contributor IV

Is there any information on typical power usage for the IMX8M-Plus and IMX8-DualXPlus SOC's ?

I know detailed power usage is very application dependent, but I would like to get a ballpark idea. So questions like:

1. What is the idle power (CPU's enabled and running) of these two SOC's with GPU and VPU enabled ?

2. What would be a reasonable full CPU usage + Graphics usage (say 25% overall CPU and displaying a H264 video) ?

3. It looks like the iMX8M-Plus will require a heat sink even for light use, how about the IMX8-DualXPlus ?

0 Kudos
1 Solution
1,354 Views
igorpadykov
NXP Employee
NXP Employee

it is AN13054.

 

Best regards
igor

View solution in original post

0 Kudos
4 Replies
1,358 Views
TerryBarnaby1
Contributor IV

Many thanks, that document is useful.

I will ask our local distributor, but do you know that there actually is an equivalent power consumption document for the IMX8M-Plus and if so what its AN number is as these is no such document on the product website ?

0 Kudos
1,355 Views
igorpadykov
NXP Employee
NXP Employee

it is AN13054.

 

Best regards
igor

0 Kudos
1,350 Views
TerryBarnaby1
Contributor IV

Many thanks.

0 Kudos
1,365 Views
igorpadykov
NXP Employee
NXP Employee

Hi TerryBarnaby1

 

>Is there any information on typical power usage for the IMX8M-Plus and IMX8-DualXPlus SOC's ?

 

one can obtaing power consumption IMX8M-Plus app note like AN12338,

through local marketing office, in general typical figures are similar to i.MX8QXP

AN12338   i.MX 8QuadXPlus Power Consumption Measurement

 

Best regards
igor

0 Kudos