IMX8M Plus Display logo during kernel (Android11_2.6.0)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M Plus Display logo during kernel (Android11_2.6.0)

Jump to solution
1,108 Views
vachlan
Contributor I

Due to the BSP(android11_2.6.0) package being  by default IMX8MP_ USES_ GKI =true。
Display drivers are loaded after kernel startup,Causing inability to display logo during kernel startup。
I will use IMX8MP_ USES_ GKI=true commented out, there was a GPU error as attached.

Please advise on how to correct the errors in this section。

 

Labels (1)
0 Kudos
1 Solution
6 Replies
1,083 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Do you want the uboot logo keep in the kernel ?

0 Kudos
1,076 Views
vachlan
Contributor I
Yes, I want to do that. But first of all, I want to display the logo in the kernel in this BSP
0 Kudos
1,085 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the NXP i.MX8MP LPDDR4 EVK board?

0 Kudos
1,075 Views
vachlan
Contributor I

Yes, we are using this board, and we have designed a similar board

0 Kudos
1,057 Views
vachlan
Contributor I
Thank you, I have read these two links you sent (which I plan to follow up on). May I ask if the IMX8MP_ USES_ GKI=true commented out。 Can GPU errors be corrected?

0 Kudos