Hi,
Could you please let me know, How to calculate the power consumption in IMX8M mini processor, I have an IMX8M mini design. The peripherals only use a camera with a CSI interface and Micro SD card. The power consumption of this design is a bit large, reaching 3.2W. So how to Reduce SoC Power when only Running A53 on i.MX8M mini.
Thank & Regards,
解決済! 解決策の投稿を見る。
Hi NXP team,
We are using 'MIMX8MM5CVTKZAA' part in our design, without VPU.
The attached Appnote AN12410 is a good reference point for our design.
Appnote provides all the relevant power consumption for 'VDD_GPU_VPU_DRAM' power supply rail. If VPU is not being used, how shall we treat power consumption on these rails.
For example, Table-3 'IDLE_DEFAULT' condition in the appnote has a total current on 'VDD_GPU_VPU_DRAM' as 402 mA.
How shall we consider the current?
1. 402 mA current on each VDD_GPU and VDD_DRAM power supply rails. 0mA on VDD_VPU.
2. 201 mA current on each VDD_GPU and VDD_DRAM rails and 0mA on VDD_VPU.
Regards,
Mihir