IMX7 SDIO detail HW guideline for layout?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX7 SDIO detail HW guideline for layout?

跳至解决方案
1,679 次查看
frankyhsu
Contributor III

We are doing the layout but we found the SDIO layout is not detail in HW design guide including the maximum length allowed and the tolerance. It should be described in detail in the HW design guide. Could you please help to have some comment for this?

Thanks.

Franky.

标签 (2)
标记 (1)
1 解答
1,290 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Franky

 

one can use ibis simulations, I am not aware of special SDIO trace length restrictions.

 

~igor

在原帖中查看解决方案

0 项奖励
6 回复数
1,290 次查看
frankyhsu
Contributor III

Hi Igor,

Got it. As you said, it will be case by case.

Thanks.

0 项奖励
1,290 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Franky

one can follow sect.3.5.8 High speed signal routing recommendations i.MX6 System
Development User’s Guide
http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
1,290 次查看
frankyhsu
Contributor III

Hi Igor,

 

The document is good for us and it includes most suggestion but we are still lack of information about the maximum SDIO allowed length and tolerance. The tolerance can be found on a HW review checking excel with a +/-50mil requirement. The maximum length become the only question we are highlighted by my customer. We use eMMC and WiFi module on SDIO bus.

 

Thanks.

0 项奖励
1,290 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Franky

document recommends :

Similar DDR rules must be followed for data, address and control as for SD module interfaces.

~igor

0 项奖励
1,290 次查看
frankyhsu
Contributor III

Hi Igor,

The DDR length defined in "IMX7DSHDG" guideline shows maximum is 1400mils for LPDDR2/3 and 1900mils for DDR3. Both 1400mil and 1900mil is small for a system application. The i.MX7 Sabre EVB also has more than 3000mil SDIO trace. That's why we do not think the value defined for DDR can not be used on SDIO case that the EVB seems also to violate it.

Thanks.

1,291 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Franky

 

one can use ibis simulations, I am not aware of special SDIO trace length restrictions.

 

~igor

0 项奖励