IMX6UL pad drive strength(DSE) for USB_OTG1_DN, USB_OTG1_DP, USB_OTG2_DN and USB_OTG2_DP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6UL pad drive strength(DSE) for USB_OTG1_DN, USB_OTG1_DP, USB_OTG2_DN and USB_OTG2_DP

Jump to solution
2,058 Views
chpub70
Contributor II

Hi NXP.

How to change the drive strength(DSE) for IM6UL pads USB_OTG1_DN, USB_OTG1_DP, USB_OTG2_DN and USB_OTG2_DP ?

Best Regards,

Pun

0 Kudos
1 Solution
2,053 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pun

 

drive strength can be configured for digital signals, not for analog as those usb signals.

For usb analog signals one can consider sect.4.3.3.2 Transmitter settings AN4589

Configuring USB on i.MX 6 Series Processors

 

Best regards
igor

View solution in original post

0 Kudos
12 Replies
2,054 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pun

 

drive strength can be configured for digital signals, not for analog as those usb signals.

For usb analog signals one can consider sect.4.3.3.2 Transmitter settings AN4589

Configuring USB on i.MX 6 Series Processors

 

Best regards
igor

0 Kudos
2,043 Views
chpub70
Contributor II

@igorpadykov ,

Hi Igor,

May I know how to change the bit of TXCAL45 of USBPHY_TX register, from Linux 3.14.52 ?

0 Kudos
2,042 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
2,029 Views
chpub70
Contributor II

@igorpadykov

Hi Igor,

I encountered on with my own board with IMX6UL, these registers cannot be accessed if there is no USB devices connected. 

Could you advise ?

 

Best Regards,

Pun

 

0 Kudos
2,022 Views
igorpadykov
NXP Employee
NXP Employee

> these registers cannot be accessed if there is no USB devices connected

 

this may be due to usb low power mode (clocks may be switched off)

 

1.jpg

 

Best regards
igor

0 Kudos
2,012 Views
chpub70
Contributor II

@igorpadykov 

Hi Igor,

Also my usb device is a full speed device. Can I still tune D_CAL, TXCAL45 because AN4589.pdf shows only for high speed device.

Thank You in advance.

Best Regards,

Pun 

0 Kudos
2,007 Views
igorpadykov
NXP Employee
NXP Employee

> Can I still tune D_CAL, TXCAL45 because AN4589.pdf shows only for high speed device.

 

I am afraid not, sorry.

 

Best regards
igor

0 Kudos
2,003 Views
chpub70
Contributor II

@igorpadykov 

Hi Igor,

You mean for full speed device has to use default value for d_cal and txcal45 ?

0 Kudos
1,999 Views
igorpadykov
NXP Employee
NXP Employee

they are used in high speed mode only.

 

Best regards
igor

0 Kudos
1,996 Views
chpub70
Contributor II

@igorpadykov 

Hi Igor,

Is there registers to tune driving current and termination resistance for full speed device ?

Do you have any recommendation to tune for USB full speed device ?

 

0 Kudos
1,992 Views
igorpadykov
NXP Employee
NXP Employee

I am afraid there are no other options, except described in application note.

 

Best regards
igor

0 Kudos
2,027 Views
chpub70
Contributor II

@igorpadykov 

Hi Igor,

Also my usb device is a full speed device. Can I still tune D_CAL, TXCAL45 because AN4589.pdf shows only for high speed device.

Thank You in advance.

Best Regards,

Pun 

0 Kudos