IMX6SX yocto setup imx_4.9.88 - booting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6SX yocto setup imx_4.9.88 - booting

933件の閲覧回数
JKT
Contributor II

Hi,

I am using IMX6SX board, and using Yocto imx_4.9.88 toolchain and linux_imx  imx_4.9.88_2.0.0_ga - from codeaurora.

After build setup done, I took the <build>/tmp/deploy/images/imx6sxsabresd/<>.sdcard.bz2, unzip it and write that to SD card using dd command.

But while booting, SD is not detected and boot fails. How to fix this?

 

============================================Log messge============

U-Boot 2017.03-imx_v2017.03_4.9.88_2.0.0_ga+gb76bb1b (Jan 09 2021 - 19:37:36 +0530)

CPU: Freescale i.MX6SX rev1.3 996 MHz (running at 792 MHz)
CPU: Extended Commercial temperature grade (-20C to 105C) at 46C
Reset cause: WDOG
Model: Freescale i.MX6 SoloX SDB RevB Board
Board: MX6SX SABRE SDB
DRAM: 1 GiB
PMIC: PFUZE100! DEV_ID=0x11 REV_ID=0x21
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
MMC: no card present
mmc_init: -123, time 1
*** Warning - MMC init failed, using default environment

Display: Hannstar-XGA (1024x768)
Video: 1024x768x18
In: serial
Out: serial
Err: serial
MMC: no card present
mmc_init: -123, time 1
Net:
Warning: ethernet@02188000 using MAC address from ROM

Warning: ethernet@021b4000 using MAC address from ROM
eth0: ethernet@02188000, eth1: ethernet@021b4000 [PRIME]
Normal Boot
Hit any key to stop autoboot: 3 2 0
=> printenv
baudrate=115200
boot_fdt=try
bootcmd=run findfdt;mmc dev ${mmcdev};mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimage; then run mmcboot; else run netboot; fi; fi; else run netboot; fi
bootcmd_mfg=run mfgtool_args; if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else bootz ${loadaddr} ${initrd_addr} ${fdt_addr}; fi;
bootdelay=3
bootscript=echo Running bootscript from mmc ...; source
console=ttymxc0
eth1addr=00:04:9f:04:5e:01
ethact=ethernet@021b4000
ethaddr=00:04:9f:04:5e:00
ethprime=eth1
fdt_addr=0x83000000
fdt_file=undefined
fdt_high=0xffffffff
fdtcontroladdr=bdf39c58
findfdt=if test $fdt_file = undefined; then setenv fdt_file imx6sx-sdb.dtb; fi;
image=zImage
initrd_addr=0x83800000
initrd_high=0xffffffff
ip_dyn=yes
loadaddr=0x80800000
loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};
loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}
loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}
loadm4image=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${m4image}
loadtee=fatload mmc ${mmcdev}:${mmcpart} ${tee_addr} ${tee_file}
m4_qspi_cs=2
m4boot=sf probe 1:${m4_qspi_cs}; bootaux 0x78000000
m4image=m4_qspi.bin
mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber=""
mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot}
mmcautodetect=yes
mmcboot=echo Booting from mmc ...; run mmcargs; if test ${tee} = yes; then run loadfdt; run loadtee; bootm ${tee_addr} - ${fdt_addr}; else if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi; fi;
mmcdev=2
mmcpart=1
mmcroot=/dev/mmcblk3p2 rootwait rw
netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${tee} = yes; then ${get_cmd} ${tee_addr} ${tee_file}; ${get_cmd} ${fdt_addr} ${fdt_file}; bootm ${tee_addr} - ${fdt_addr}; else if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;fi;
panel=Hannstar-XGA
script=boot.scr
tee=no
tee_addr=0x84000000
tee_file=uTee-6sxsdb
update_m4_from_sd=if sf probe 1:${m4_qspi_cs}; then if run loadm4image; then setexpr fw_sz ${filesize} + 0xffff; setexpr fw_sz ${fw_sz} / 0x10000; setexpr fw_sz ${fw_sz} * 0x10000; sf erase 0x0 ${fw_sz}; sf write ${loadaddr} 0x0 ${filesize}; fi; fi

Environment size: 3077/8188 bytes
=>

 

0 件の賞賛
7 返答(返信)

929件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the 6sx sabre board from NXP or the board you design yourself?

0 件の賞賛

923件の閲覧回数
JKT
Contributor II

I am using board from NXP.

0 件の賞賛

929件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Does the kernel boot up?

0 件の賞賛

922件の閲覧回数
JKT
Contributor II

NO it does not bootup. Stuck at Uboot level.

0 件の賞賛

920件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

How do you set the kernel boot command line in u-boot?

0 件の賞賛

916件の閲覧回数
JKT
Contributor II

I did not set any yet. By default it boots from SD card right?

Could you please provide the possible options to fix/test this? Its a bit urgent.

0 件の賞賛

899件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, you can see the section 4.7 Running Linux OS on the target of our user guide, following the use guide setting. If can not work tell me.

0 件の賞賛