IMX6SX ref design / kernel support for 14x14 package ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6SX ref design / kernel support for 14x14 package ?

688 Views
SJA
Contributor II

Is there a reference design / schematics symbols for the IMX6SX (Solo X) in the 14x14 package ??

Also what about a kernel DTS/DTB file for the 14x14 package ??

Looks like u-boot supports it (make mx6sx_14x14_lpddr2_arm2_defconfig) ....

But I do not see any imx6sx-14x14... dts files in the kernel tree under arch/arm/boot/dts

Labels (1)
0 Kudos
Reply
1 Reply

493 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Stuart.

Attached you could find the symbols and footprints for the i.MX6SX in MAPBGA400 package (14x14).

Regarding the DTB, you could use as reference the DTS from the official BSPs, and removing the modules that are not included on the target package, for compiling and generating a proper DTB file.


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply