Dear,
I am trying to setup a custom display (320X480,RGB666) on a custom board based on IMX6SLEVK and I am facing some problems.
I am porting the Android-JB in my custom board.
Custom display Details:
Display =(320 X RGB X 480 dots), Driver IC = ILI9488, Backlight Type= LED, Interface = 80-series CPU 8/9/16/18 bit selectable,RGB 6/16/18 bit ,3/4 serial.
I added codes in board-mx6sl_evk.c file for custom lcd .
static struct fb_videomode wvga_video_modes[] = {
{
// 320x480 @ 60 Hz
"MY-LCD", 60, 320, 480, 29850, 89, 164, 23, 10, 10, 10,
FB_SYNC_CLK_LAT_FALL,
FB_VMODE_NONINTERLACED,
0,},
{
// 800x480 @ 57 Hz , pixel clk @ 32MHz
"SEIKO-WVGA", 60, 800, 480, 29850, 89, 164, 23, 10, 10, 10,
FB_SYNC_CLK_LAT_FALL,
FB_VMODE_NONINTERLACED,
0,},
};
static struct mxc_fb_platform_data wvga1_fb_data[] = {
{
.interface_pix_fmt = V4L2_PIX_FMT_BGR666,
.mode_str = "MY-LCD",
.mode = wvga_video_modes,
.num_modes = ARRAY_SIZE(wvga_video_modes),
},
};
static struct platform_device lcd_wvga1_device = {
.name = "lcd_mine",
};
mxc_register_device(&lcd_wvga1_device, NULL); // Added in mx6_evk_init function
// I created the LCD driver is mxc_my_lcd.c based on the mxc_seiko_wvga.c . I just changed the resolutions and lcd driver structure in mxc_my_lcd.c
static struct platform_driver lcd_driver = {
.driver = {
.name = "lcd_mine"},
.probe = lcd_probe,
.remove = __devexit_p(lcd_remove),
.suspend = lcd_suspend,
.resume = lcd_resume,
};
//and then add The LCD's driver is at path linux/drivers/video/mxc/mxc_my_lcd.c .and compiled it successfully
then i booted the board log comes like :
" mxc_elcdif_fb mxc_elcdif_fb: ELCDIF unsupported output pixel format 1213351746
warning: `zygote' uses 32-bit capabilities (legacy support in use)
request_suspend_state: wakeup (3->0) at 16063640921 (1970-01-02 00:02:19.478720753 UTC)
acc_open
acc_release
init: sys_prop: permission denied uid:1003 name:service.bootanim.exit
mxc_elcdif_fb mxc_elcdif_fb: can't wait for VSYNC when fb is blank
request_suspend_state: sleep (0->3) at 79646326887 (1970-01-02 00:03:23.061406677 UTC) "
I attached log of my custom board, mxc_my_lcd.c and U-boot environmrnt variables .Please Find it.
Thanks and Regards,
vinothraj m
Original Attachment has been moved to: log.txt.zip
Original Attachment has been moved to: mxcfb_my_lcd.c.txt.zip
Original Attachment has been moved to: Env_Variable.txt.zip
Hi,
the rgb format is wrong
/kernel/include/linux/videodev2.h
#define V4L2_PIX_FMT_RGB666 v4l2_fourcc('R', 'G', 'B', '6') /* 18 RGB-6-6-6 */
#define V4L2_PIX_FMT_BGR666 v4l2_fourcc('B', 'G', 'R', '6') /* 18 BGR-6-6-6 */
and ili9488 is 8080 mpu lcd driver
How to support the i80 MPU interface LCD on iMX50 Linux platform -blog archive
Hi vinothraj
for 80-series interface lcd support please check i.MX28 LCDIF patch
(i.MX6SL eLCDIF is similar module)
Patch for i.MX28's 8080 mode Lcd panel driver
Best regards
igor