I found the power-up sequence restrictions in 4.2.1 Power-Up Sequence of IMX6SDLIEC.pdf.
My customer not use external SRC_POR_B signal(left unconnected) and also not use PMIC design. Other design is refer to SPF-27516_C3.pdf(Sabre_sdb Schematics).
Their design's power-up sequence is also not same with SPF-27516_C3.pdf(Sabre_sdb Schematics).
1)Customer's 1.425V supply(VDD_SOC/VDD_ARM_IN) power up after the DDR3 supply(the sequence is not the same with the Sabre_sdb supply sequence).
2)In Sabre_sdb supply sequence, DDR_VREF power up in the same sequence with DDR_1.5V. But in customer's design, VREFDDR0.75V power up before DDR3 1.5V supply(more than 14.5ms).
I don't know whether the sequence is OK as I can not find any restrictions information for the case.
Thank you for your help and look forward to your kindly answer.
解決済! 解決策の投稿を見る。
I think Your power up sequence can violate the next restriction :
All i.MX6 I/O pins should not be externally driven while the I/O power supply
for the pin (NVCC_xxx) is OFF. This can cause internal latch-up and malfunctions
due to reverse current flows.
The recommended power up sequence (agree - it is not clearly described) is as following :
1) VDD_SNVS_IN (+optional VDD_HIGH_IN)
2) VDD_ARMx_IN / VDD_SOC_IN
3) all other supplies.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I think Your power up sequence can violate the next restriction :
All i.MX6 I/O pins should not be externally driven while the I/O power supply
for the pin (NVCC_xxx) is OFF. This can cause internal latch-up and malfunctions
due to reverse current flows.
The recommended power up sequence (agree - it is not clearly described) is as following :
1) VDD_SNVS_IN (+optional VDD_HIGH_IN)
2) VDD_ARMx_IN / VDD_SOC_IN
3) all other supplies.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
Thank you for your kindly answer.
Could you help to give a reason about the VDD_ARMx_IN / VDD_SOC_IN should be power-up before all other supplies except VDD_SNVS_IN?
Providing VDD_ARMx_IN / VDD_SOC_IN power-up before all other supplies allows to avoid unpredictable
(GPIO) pin states during power up.
~Yuri.