IMX6S: USB OTG Not working in slave mode on imx6s

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6S: USB OTG Not working in slave mode on imx6s

1,113件の閲覧回数
muthumani
Contributor I

I am working with imx6 solo processor with a custom base board which is running android kk 4.4.2.

We have a USB 2.0 HUB connected to SOM on USB_HOST_DP, USB_HOST_DN.

And OTG is connected independent from USB 2.0 HUB to SOM.

When we tried to switch OFF and ON the power to USB 2.0 HUB (which is a GPIO from SOM), peripherals connected to USB HUB is working fine.

When OTG is in slave mode android is not able to work in fastboot / adb.

But it is able to work in HOST mode.

Regards,

M.Muthumani.

ラベル(2)
0 件の賞賛
1 返信

685件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Muthumani

for USB OTG one can check if USB connector ID pin is floating

and voltage on porcessor VDD_VBUS_CAP.

Please check also attached document sect.8.2 How do I use Android

fastboot? It makes sense to check OTG in slave mode using MFG Tools:

will it connect and probably with Linux.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛